MIMX8ML8CVNKZAB Thermal Management

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMX8ML8CVNKZAB Thermal Management

1,852 Views
Pavanecon
Contributor II

Hi Team,

We developed a customized board for our application with MIMX8ML8CVNKZAB SOC. During our thermal test, we observed that at 55 °C, our board is getting shutdown. This is due to the default thermal shutdown at 95 °C junction temperature.

As per the reference manual, the SOC Thermal Shutdown temperature can be configured up to 105C.

Now we are planning to configure the thermal shutdown temperature to 100 °C.

So, is it worth changing the thermal shutdown temperature to 100 °C? or do we have any risk of doing this?

Can NXP provide any views or comments on this?

Labels (1)
0 Kudos
Reply
3 Replies

1,789 Views
Pavanecon
Contributor II

Hi Joanxie,

Thanks for the reply

0 Kudos
Reply

1,825 Views
Pavanecon
Contributor II
Is it safe to change the thermal shutdown temperature to 100 C? Can anyone reply on this
0 Kudos
Reply

1,819 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the data sheet, industrial can support up to the 105

joanxie_0-1726708185871.png

but consider the margin 10°C to the max temperature, we suggest customer set 95°C as critical temperature, which not mean the 100 is not allowed, just consider the sensor accuracy

0 Kudos
Reply