MII Connection problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MII Connection problem

2,857 次查看
alessandromaggi
Contributor I

Hi,

I have a custom board(designed by us) based on IMX6 SoloX. This board has (among other) two optical ports 100-FX, realized connecting a micrel KSZ8873FLLI via MII to the SoloX.

The problem is that I found an unexpected electrical level on the MII interface in TX direction. I would like the high level to be 3.3V, but on the oscilloscope I quite often can see a stable level around 2 volts.

So on the TX line I can see 3 different voltage level: 3.3V (expected igh level), 2V (unexpected and unwanted high level), and 0V (low level).

Of course with this condition the port is not working.

My question are:

1) Is it possibile for the SoloX to work with an MII interface with 3.3V as high level ? The reference manual is not very clear on this topic.

2) If yes, how the NVCC_SGMII should be connected ?

3) What can cause this strange 3 level signal ?

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

2,662 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  Alessandro

one can recheck enet power supplies connections using

i.MX6SX Datasheet Table 110. 19x19 mm Functional Contact Assignments

"Power Group" column
https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf

Also one can look for layout errors and short circuit between traces.

3.3V is allowable value according to Table 10. Operating Ranges i.MX6SX Datasheet.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复