MFGTool2 get MAC address on error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFGTool2 get MAC address on error

590件の閲覧回数
Alex_S
Contributor I

I am using MFGTool2 (ucl2.xml) for burning 4 devices at the same time. I would like to get the MAC address of the device if any of the processes does not success. I have tried to obtain the MAC address on a .txt before and after the proccess to compare it later with the following comand:

<CMD state="Updater" type="push" body="read [.txt with the MAC]" savedfile="MAC.txt">Obtaining MAC</CMD>

Since the 4 processes happen paralelly the .txt is overwritten resulting in only the last MAC address. I have not found much info of ucl2 commands.

So is it possible to just append the MAC instead of overwrite it to the .txt or just to get the .txt when an error occurs?

Thanks

ラベル(1)
0 件の賞賛
返信
0 返答(返信)