MFGTool: push command alwais fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFGTool: push command alwais fail

8,635 Views
BrilliantovKiri
Senior Contributor I

Hello!

I use MFGTool 1.6.2.0.42-g92b97ee and uuc-11.09.01 from LTIB, now I try write all components on NAND.

My ucl.xml:

<LIST name="MobileCam-NAND" desc="Flash system on NAND">

        <CMD type="boot" body="BootStrap" file ="u-boot_mfg.bin" >Load U-Boot.</CMD>

        <CMD type="load" file="uImage" address="0x70800000" loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" >Load Linux.</CMD>

        <CMD type="load" file="initramfs.img" address="0x70B00000" loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" >Doing Initramfs.</CMD>

        <CMD type="jump" >Jumping to OS image.</CMD>

        <CMD type="find" body="Updater" timeout="180"/>

        <CMD type="push" body="send" file="uImage">Send uImage</CMD>

        <CMD type="push" body="$ /root/flash_erase /dev/mtd2 0 0">Erase /dev/mtd2</CMD>

        <CMD type="push" body="$ /root/nandwrite -mp /dev/mtd2" file="uImage">Write Linux on /dev/mtd2</CMD>

        <CMD type="push" body="$ /root/flash_erase /dev/mtd3 0 0">Erase /dev/mtd3</CMD>

        <CMD type="push" body="$ /root/nandwrite -mp /dev/mtd3" file="uImage">Write Linux on /dev/mtd3</CMD>

        <CMD type="push" body="$ mkdir /mnt">Create mount point</CMD>

        <CMD type="push" body="$ mount -t jffs2 /dev/mtdblock4 /mnt">Mount /dev/mtdblock4 to /mnt</CMD>

        <CMD type="push" body="$ rm -rf /mnt/*">Erase /dev/mtdblock4</CMD>

        <CMD type="push" body="pipe tar -xv -C /mnt" file="rootfs.tar">Unpack rootfs</CMD>

        <CMD type="push" body="$ umount /mnt">Umount /mnt</CMD>

</LIST>

Unfortunally all stopped on first push command.

Via console I not see any error:
UTP: received command '$ /root/flash_erase /dev/mtd2 0 0'
UTP: executing "/root/flash_erase /dev/mtd2 0 0"
Erasing 128 Kibyte @ 3e0000 -- 100 % complete
UTP: sending Success to kernel for command $ /root/flash_erase /dev/mtd2 0 0.

But in log:

Panel A Start <CMD/> type="push" body="$ /root/flash_erase /dev/mtd2 0 0" file="" timeout="10" onError="" text="Erase /dev/mtd2".

1 - Panel A Finished <CMD/> type="push" body="$ /root/flash_erase /dev/mtd2 0 0" file="" timeout="10" onError="" text="Erase /dev/mtd2" FAIL code=-1.

Panel A: failed to run command: type="push" body="$ /root/flash_erase /dev/mtd2 0 0" file="" timeout="10" onError="" text="Erase /dev/mtd2" ,, Error code:-1

I not understand this. I try change all shell command on pipe and this work for flashing Linux, I think, but this not work for unpack rootfs, I always found rootfs in directory /mnt, not on NAND.

I try use flush command for wait mount, unfortunally it not work, uuc not know it:

Panel A Start <CMD/> type="push" body="flush" file="" timeout="10" onError="" text="Wait mount /dev/mtdblock4".

1 - Panel A Finished <CMD/> type="push" body="flush" file="" timeout="10" onError="" text="Wait mount /dev/mtdblock4" FAIL code=-1.

Panel A: failed to run command: type="push" body="flush" file="" timeout="10" onError="" text="Wait mount /dev/mtdblock4" ,, Error code:-1

Why all console commands fail and how can I solve this problem?

Thank you and excuse me my bad englsih.

Labels (1)
Tags (2)
0 Kudos
Reply
18 Replies

5,824 Views
luwinbo
Contributor III

Maybe it's a hardware issue. I had the same issue, and last the reason we found is hardware interference.

0 Kudos
Reply

5,824 Views
BrilliantovKiri
Senior Contributor I

One moment about my configuration - MFGTool work in WindowsXP under VirtualBox, host system Debian GNU/Linux.

0 Kudos
Reply

5,824 Views
israelpz
Senior Contributor I

Hi Kirill,

Before this issue happen, had you were be able to write a image using mfgtool?

Looking in your log seem the UTP message is arriving and the board confirm the packet is valid. I don't have right now a clear idea why the first push command is failing.

I going to try a similar configuration and check if this issue happens.

Regards,

-Israel.

0 Kudos
Reply

5,824 Views
BrilliantovKiri
Senior Contributor I

Hello, Israel!

Unfortunally I can't success story for writing system on NAND via MFGTool, but on seminar I see what MFGtool can write system on SD-card QuickStartBoard-R.

0 Kudos
Reply

5,824 Views
israelpz
Senior Contributor I

Hi Kirill,

I had been trying to reproduce the issue but i don't got any issue with the push command.

Did you try to reproduce your issue in a PC with Windows as native OS?

Regards,

-Israel.

0 Kudos
Reply

5,824 Views
BrilliantovKiri
Senior Contributor I

Hello, Israel!

I will try found PC with Windows for this test.

P.S. May be FreeScale rewrite MfgTool for work on Linux also, e.g. on Qt? I not think what this very hard.

0 Kudos
Reply

5,824 Views
YixingKong
Senior Contributor IV

Kirill

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

5,824 Views
BrilliantovKiri
Senior Contributor I

Hello!

Problem not solved but now I havn't time for this problem.

0 Kudos
Reply

5,824 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Kirill,

when you have time to  work on this  case please let us know to continue with it

0 Kudos
Reply

5,824 Views
israelpz
Senior Contributor I

Kirill,

Could you post the kernel log?

Looks also you kernel doesn't have USB gadget UTP support.

Regards,

-Israel.

0 Kudos
Reply

5,824 Views
BrilliantovKiri
Senior Contributor I

Hello, Israel!

Follow Linux log:

Linux version 2.6.35.3+ (kirill@kirill) (gcc version 4.4.4 (4.4.4_09.06.2010) )4

CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7f

CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache

Machine: Byterg MX53 MobileCam

Memory policy: ECC disabled, Data cache writeback

On node 0 totalpages: 122880

free_area_init_node: node 0, pgdat 804722bc, node_mem_map 80e84000

  DMA zone: 224 pages used for memmap

  DMA zone: 0 pages reserved

  DMA zone: 28448 pages, LIFO batch:7

  Normal zone: 2336 pages used for memmap

  Normal zone: 91872 pages, LIFO batch:31

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 120320

Kernel command line: console=ttymxc1,115200 rdinit=/linuxrc root=/dev/mtdblock4t

PID hash table entries: 2048 (order: 1, 8192 bytes)

Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

Memory: 224MB 256MB = 480MB total

Memory: 478932k/478932k available, 12588k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xf8e00000 - 0xffe00000   ( 112 MB)

    vmalloc : 0xd0800000 - 0xf4000000   ( 568 MB)

    lowmem  : 0x80000000 - 0xd0000000   (1280 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .init : 0x80008000 - 0x80028000   ( 128 kB)

      .text : 0x80028000 - 0x80425000   (4084 kB)

      .data : 0x8043c000 - 0x80473020   ( 221 kB)

SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

Hierarchical RCU implementation.

        RCU-based detection of stalled CPUs is disabled.

        Verbose stalled-CPUs detection is disabled.

NR_IRQS:368

MXC GPIO hardware

MXC IRQ initialized

MXC_Early serial console at MMIO 0x53fc0000 (options '115200')

bootconsole [ttymxc1] enabled

Calibrating delay loop... 159.74 BogoMIPS (lpj=798720)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

devtmpfs: initialized

regulator: core version 0.5

NET: Registered protocol family 16

i.MX IRAM pool: 128 KB@0xd0840000

IRAM READY

CPU is i.MX53 Revision 2.1

Using SDMA I.API

MXC DMA API initialized

IMX usb wakeup probe

the wakeup pdata is 0x80449608

IMX usb wakeup probe

the wakeup pdata is 0x804496bc

bio: create slab <bio-0> at 0

SCSI subsystem initialized

libata version 3.00 loaded.

Freescale USB OTG Driver loaded, $Revision: 1.55 $

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

24bit read error, ret = -5

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

IP route cache hash table entries: 4096 (order: 2, 16384 bytes)

TCP established hash table entries: 16384 (order: 5, 131072 bytes)

TCP bind hash table entries: 16384 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 16384 bind 16384)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Unpacking initramfs...

Freeing initrd memory: 3596K

LPMode driver module loaded

Static Power Management for Freescale i.MX5

PM driver module loaded

sdram autogating driver module loaded

Bus freq driver module loaded

mxc_dvfs_core_probe

mxc_dvfs_core_probe: failed to get gp regulator

DVFS driver module loaded

i.MXC CPU frequency driver

mxc_cpufreq_driver_init: failed to get gp regulator

DVFS PER driver module loaded

NTFS driver 2.1.29 [Flags: R/W].

JFFS2 version 2.2. (NAND) �� 2001-2006 Red Hat, Inc.

fuse init (API version 7.14)

msgmni has been set to 942

alg: No test for stdrng (krng)

cryptodev: driver loaded.

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

Serial: MXC Internal UART driver

mxcintuart.0: ttymxc0 at MMIO 0x53fbc000 (irq = 31) is a Freescale i.MX

mxcintuart.1: ttymxc1 at MMIO 0x53fc0000 (irq = 32) is a Freescale i.MX

console [ttymxc1] enabled, bootconsole disabled

mxcintuart.2: ttymxc2 at MMIO 0x5000c000 (irq = 33) is a Freescale i.MX

mxcintuart.3: ttymxc3 at MMIO 0x53ff0000 (irq = 13) is a Freescale i.MX

mxcintuart.4: ttymxc4 at MMIO 0x63f90000 (irq = 86) is a Freescale i.MX

Wait for CR ACK error!

ahci: probe of ahci.0 failed with error -5

MXC MTD nand Driver 3.0

NAND device: Manufacturer ID: 0x2c, Chip ID: 0xba (Micron NAND 256MiB 1,8V 16-b)

Bad block table found at page 1048512, version 0x01

Bad block table found at page 1048448, version 0x01

RedBoot partition parsing not available

Creating 6 MTD partitions on "NAND 256MiB 1,8V 16-bit":

0x000000000000-0x000001000000 : "bootloader"

0x000001000000-0x000001080000 : "params"

0x000001080000-0x000001480000 : "kernel"

0x000001480000-0x000001880000 : "kernel2"

0x000001880000-0x000009880000 : "filesystem"

0x000009880000-0x000080000000 : "filesystem2"

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 18, io base 0x53f80000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

fsl-ehci fsl-ehci.1: irq 14, io base 0x53f80200

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

ARC USBOTG Device Controller driver (1 August 2005)

i2c /dev entries driver

Linux video capture interface: v2.00

mxc_v4l2_output mxc_v4l2_output.0: Registered device video0

APM Battery Driver

MXC WatchDog Driver 2.0

MXC Watchdog # 0 Timer: initial timeout 60 sec

PMIC Character device: successfully loaded

VPU initialized

gpu mmu enabled

mxsdhci: MXC Secure Digital Host Controller Interface driver

mxsdhci: MXC SDHCI Controller Driver.

mmc0: SDHCI detect irq 0 irq 1 INTERNAL DMA

TCP cubic registered

NET: Registered protocol family 17

VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 2

Freeing init memory: 128K

mmc0: new high speed SDHC card at address 0007

mmcblk0: mmc0:0007 SD32G 29.3 GiB

mmcblk0: p1

USB Host suspend begins

will suspend roothub and its children

ehci_fsl_bus_suspend, DR

host suspend ends

ehci_fsl_bus_suspend, Host 1

check_parameters:UTP settings are in place now, overriding defaults

g_file_storage gadget: File-backed Storage Gadget, version: 20 November 2008

g_file_storage gadget: Number of LUNs=1

Suspend udc for OTG auto detect

USB Gadget resume begins

dr_controller_run: udc out low power mode

USB Gadget resume ends

fsl-usb2-udc: bind to driver g_file_storage

g_file_storage gadget: high speed config #1

And UTP log:

UTP: received command 'send'

UTP: sending Success to kernel for command send.

UTP: received command '$ /root/flash_system.sh -Ll $FILE'

UTP: executing "/root/flash_system.sh -Ll $FILE"

Write Linux on NAND /dev/mtd2

Erasing 128 Kibyte @ 3e0000 -- 100 % complete

Writing data to block 0 at offset 0x0

Writing data to block 1 at offset 0x20000

Writing data to block 2 at offset 0x40000

Writing data to block 3 at offset 0x60000

Writing data to block 4 at offset 0x80000

Writing data to block 5 at offset 0xa0000

Writing data to block 6 at offset 0xc0000

Writing data to block 7 at offset 0xe0000

Writing data to block 8 at offset 0x100000

Writing data to block 9 at offset 0x120000

Writing data to block 10 at offset 0x140000

Writing data to block 11 at offset 0x160000

Writing data to block 12 at offset 0x180000

Writing data to block 13 at offset 0x1a0000

Writing data to block 14 at offset 0x1c0000

Writing data to block 15 at offset 0x1e0000

Writing data to block 16 at offset 0x200000

Writing data to block 17 at offset 0x220000

Write second Linux on NAND /dev/mtd3

Erasing 128 Kibyte @ 3e0000 -- 100 % complete

Writing data to block 0 at offset 0x0

Writing data to block 1 at offset 0x20000

Writing data to block 2 at offset 0x40000

Writing data to block 3 at offset 0x60000

Writing data to block 4 at offset 0x80000

Writing data to block 5 at offset 0xa0000

Writing data to block 6 at offset 0xc0000

Writing data to block 7 at offset 0xe0000

Writing data to block 8 at offset 0x100000

Writing data to block 9 at offset 0x120000

Writing data to block 10 at offset 0x140000

Writing data to block 11 at offset 0x160000

Writing data to block 12 at offset 0x180000

Writing data to block 13 at offset 0x1a0000

Writing data to block 14 at offset 0x1c0000

Writing data to block 15 at offset 0x1e0000

Writing data to block 16 at offset 0x200000

Writing data to block 17 at offset 0x220000

UTP: sending Success to kernel for command $ /root/flash_system.sh -Ll $FILE.

0 Kudos
Reply

5,824 Views
BrilliantovKiri
Senior Contributor I

Hello, Israel!

I can post kernel log, but I think you not right because first post contained UTP console output:

UTP: received command '$ /root/flash_erase /dev/mtd2 0 0'
UTP: executing "/root/flash_erase /dev/mtd2 0 0"
Erasing 128 Kibyte @ 3e0000 -- 100 % complete
UTP: sending Success to kernel for command $ /root/flash_erase /dev/mtd2 0 0.

0 Kudos
Reply

5,824 Views
Yuri
NXP Employee
NXP Employee

flash_erase operation may require some time. Perhaps the problem is caused by timeout in communications

between MFG and updater. Please try to use parameter "timeout" in push CMD in order to prolong waiting.   

0 Kudos
Reply

5,824 Views
BrilliantovKiri
Senior Contributor I

Hello, Yuri!

From log:

1 - Panel A Finished <CMD/> type="push" body="$ /root/flash_erase /dev/mtd2 0 0" file="" timeout="10" onError="" text="Erase /dev/mtd2" FAIL code=-1.

flash_erase work time is less then 10 sec, it work 1 sec

I also try simple command, e.g. "echo Write complete!" and it also stop with error.

0 Kudos
Reply

5,824 Views
YixingKong
Senior Contributor IV

Kirill

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel free to contact Freescale.

Thanks,
Yixing

0 Kudos
Reply

5,824 Views
BrilliantovKiri
Senior Contributor I

Hello, Yixing Kong!

Unfortunally problem not solved, but I not try solve it again after my last post.

0 Kudos
Reply

5,824 Views
YixingKong
Senior Contributor IV

Kirill

Freescale experter had below comment:

"Wait for pipe finish transfer before umount."

If yu still have any further questions please reply this message by an update.

Thanks,

Yixing

0 Kudos
Reply

5,824 Views
BrilliantovKiri
Senior Contributor I

Hello, Yixing!

I try return to this problem on next week and recheck all my steps.

0 Kudos
Reply