Hi All,
I download MFG tool form official web site and try to upgrade my board, i do some ddr configuration for my board. But MFG always stop on "UTP: Waiting for device to appear". The full log and MFG log as attached.
How to resolve it ? Thanks!
Original Attachment has been moved to: MfgTool.log.zip
Original Attachment has been moved to: MFG-Android6_Log.txt.zip
Hi David
in hardware one can check usb_id signal, should be float or high,
processor USB_OTG_VBUS should has power. In software one
can check if usb functionality works running linux minimal image
and unit tests (imx-test/../mxc_usb_test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
USB_OTG_VBUS is 5V and usb_id (ENET_RX_ER) is floating. And The board is working fine in Android 5.x (MFG tools)... Do have some guide of the Test tools ? I don't understand how to use it. Thanks!
BR.
David
Hi David
what do you mean by "Test tools" ?
Regarding mfg tools one can check documentation in
ga-mfg-tools/Document folder.
Best regards
igor
Hi Igor,
The test tools is "(imx-test/../mxc_usb_test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz" your share to me....
Acturely the board is working fine on Android 5 and MFG tools version "L5.1_2.1.0"..
Maybe I can tryto modify zImage to fix it. But I can't get string "Starting UTP" or "UTP:" by grep....
Does that is part of android source ? Thanks!
BR.
David Wu
Hi David
documentation is included in doc folder of imx-test/../mxc_usb_test/doc
Best regards
igor