MFG tool got stuck at "Loading u-boot"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG tool got stuck at "Loading u-boot"

988 Views
vijayansivamani
Contributor II

This is the custom board based on i.MX6 processor. There are few boards (out of thousands) got failed on MFG tool. It got stuck at "Loading u-boot". This should be hardware issue. But here I would like to know, in this case, there is good chance that processor can't able to communicate RAM properly. 

For debugging, can I use DDR stress test tool.. If test failed, I can  say that the issue is with memory malfunction (assembly issue or any other)... Is this enough or can I do any other testing for identifying the root cause ?

-Vijay

0 Kudos
Reply
1 Reply

760 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Vijay,

The stress tool is a very good way of finding if there is a problem with the PCB, but it may be caused by a problem with the design or of the manufacture. Besides reviewing your PCB design, especially DDR and power rails, I would also recommend reviewing the PCB through an X-ray machine to make sure that there were no problems on the manufacturing process.

I hope this helps!

Regards,

0 Kudos
Reply