MFG Tool hangs for custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG Tool hangs for custom board

1,684 Views
mukelarvin
Contributor IV

Hi I'm trying to get the MFG Tool to program an SD card in my custom board. I've got the DDR and u-boot set up correctly but the output hangs.

I've posted the log in a gist:

https://gist.github.com/3fec0ebd75579eac57e6.git

It hangs after:

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

When I use the MFG Tool with the reference design we used the next lines in the log are:

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

----enable clko2

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.

hw-breakpoint: maximum watchpoint size is 4 bytes.

Is my board getting stuck in this hw-breakpoint? I'm just using the standard uImage that was in the MFG Tool directory.

Labels (2)
0 Kudos
Reply
1 Reply

1,438 Views
igorpadykov
NXP Employee
NXP Employee

Hi Luke

had you rebuilt mfg tools firmware, this is described in attached

Yocto Guide sect.6.2 Manufacturing Tool, MFGTool.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply