MFG Tool Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG Tool Issue

Jump to solution
1,404 Views
tony_l_cai
Contributor III

Hi All,

     when I used MFG Tool download the img to the board, The prompt stopped on the "Loading uboot",and didn't continue to the follow steps. What has happened?

     And what I need to do can make all work? please help me in detail. 3Q!

Labels (2)
0 Kudos
Reply
1 Solution
1,182 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

for new board please run DDR test

https://community.freescale.com/docs/DOC-96412

and rebuild MFG Tools with new board ddr settings in Uboot file flash_header.S

check sect.3.9 Building Manufacturing Firmware attached document

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,183 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

for new board please run DDR test

https://community.freescale.com/docs/DOC-96412

and rebuild MFG Tools with new board ddr settings in Uboot file flash_header.S

check sect.3.9 Building Manufacturing Firmware attached document

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,182 Views
tony_l_cai
Contributor III

The following picture is the operation after DDR stress tool testing:

1.bmp

and could you tell me some possible reasons?

0 Kudos
Reply
1,182 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

for new problem/qustion new thread should be

created.

Thanks !

~igor

0 Kudos
Reply