Hi. everyone.
Our custom board based on i.MX6SL(SoloLite) EVK board and using MCIMX6L8DVN10AB.
(platform : imx-3.10.17-1.0.0_ga, Boot CFG: eMMC using uSDHC2, LPDDR2, without LCD)
Recently our custom i.mx6SL board wanna using eMMC 5.1 instead eMMC 4.4.
Now i try to use MFG tool to download firmware to eMMC 5.1, But always fail. the log as below(refer attachment file):
Could some one give me some hint?
Thanks.
-------------------------------------------------------------------------------------------------------------
U-Boot 2013.04 (Oct 10 2014 - 12:25:37)
CPU: Freescale i.MX6SL rev1.2 at 792 MHz
CPU: Temperature 41 C, calibration data: 0x5a151d5f
Reset cause: POR
Board: MX6SLEVK
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
MMC: no card present
MMC init failed
Using default environment
In: serial
Out: serial
Err: serial
Found PFUZE100! deviceid=10,revid=21
MMC: no card present
mmc0(part 0) is current device
Net: FEC [PRIME]
Warning: failed to set MAC address
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootm ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
## Booting kernel from Legacy Image at 80800000 ...
Image Name: Linux-3.10.17-1.0.0_ga+g232293e
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5300504 Bytes = 5.1 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 83800000 ...
Image Name: initramfs
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 4399687 Bytes = 4.2 MiB
Load Address: 12c00000
Entry Point: 12c00000
Verifying Checksum ... OK
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Loading Kernel Image ... OK
OK
switch to ldo_bypass mode!
Using Device Tree in place at 83000000, end 8300b524
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 3.10.17-1.0.0_ga+g232293e (korea@korea-H67M-D2-B3-2) (gcc version 4.8.1 (GCC) ) #2 SMP PREEMPT Fri Oct 10 12:13:04 KST 2014
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX6 SoloLite (Device Tree), model: Freescale i.MX6 SoloLite EVK Board
cma: CMA: reserved 320 MiB at 8c000000
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 8 pages/cpu @8111e000 s8896 r8192 d15680 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber=
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 512MB = 512MB total
Memory: 173644k/173644k available, 350644k reserved, 0K highmem
................................... [skip] ...................................
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
mmc1: unrecognised EXT_CSD revision 8
mmc1: error -22 whilst initialising MMC card
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh mksdcard.sh /dev/mmcblk0'
UTP: executing "sh mksdcard.sh /dev/mmcblk0"
1+0 records in
1+0 records out
sfdisk: Warning: /dev/mmcblk0 is not a block device
sfdisk: Disk /dev/mmcblk0: cannot get geometry
Disk /dev/mmcblk0: 0 cylinders, 255 heads, 63 sectors/track
sfdisk: /dev/mmcblk0: unrecognized partition table type
Old situation:
sfdisk: No partitions found
Warning: given size (0) exceeds max allowable size (503)
New situation:
Units: 1MiB = 1024*1024 bytes, blocks of 1024 bytes, counting from 0
Device Boot Start End MiB #blocks Id System
/dev/mmcblk0p1 7+ 509- 503- 514080 c W95 FAT32 (LBA)
/dev/mmcblk0p2 596+ 596- 0 0 83 Linux
/dev/mmcblk0p3 0 - 0 0 0 Empty
/dev/mmcblk0p4 0 - 0 0 0 Empty
Warning: partition 2 has size 0 but is not marked Empty
Warning: partition 1 extends past end of disk
Successfully wrote the new partition table
If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
UTP: sending Success to kernel for command $ sh mksdcard.sh /dev/mmcblk0.
utp_poll: pass returned.
mmc1: unrecognised EXT_CSD revision 8
mmc1: error -22 whilst initialising MMC card
mmc1: unrecognised EXT_CSD revision 8
mmc1: error -22 whilst initialising MMC card
mmc1: unrecognised EXT_CSD revision 8
mmc1: error -22 whilst initialising MMC card
UTP: received command 'send'
UTP: sending Success to kernel for command send.
mmc1: unrecognised EXT_CSD revision 8
mmc1: error -22 whilst initialising MMC card
UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk0 bs=1k seek=384 conv=fsync count=129'
UTP: executing "dd if=/dev/zero of=/dev/mmcblk0 bs=1k seek=384 conv=fsync count=129"
129+0 records in
129+0 records out
UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk0 bs=1k seek=384 conv=fsync count=129.
utp_poll: pass returned.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk0 bs=1k seek=1 conv=fsync'
UTP: executing "dd if=$FILE of=/dev/mmcblk0 bs=1k seek=1 conv=fsync"
281+1 records in
281+1 records out
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk0 bs=1k seek=1 conv=fsync.
utp_poll: pass returned.
UTP: received command '$ mkfs.vfat /dev/mmcblk0p1'
UTP: executing "mkfs.vfat /dev/mmcblk0p1"
mkfs.vfat 2.11 (12 Mar 2005)
/dev/mmcblk0p1: No such file or directory
UTP: sending Non-success to kernel for command $ mkfs.vfat /dev/mmcblk0p1.
utp_poll: exit with status 256
mmc1: unrecognised EXT_CSD revision 8
mmc1: error -22 whilst initialising MMC card
mmc1: unrecognised EXT_CSD revision 8
mmc1: error -22 whilst initialising MMC card
mmc1: unrecognised EXT_CSD revision 8
................................... [skip] ...................................
-------------------------------------------------------------------------------------------------------------------------
( Note: I have made initramfs.cpio.gz.boot for mfgtool.
1. changed mmc.c by "https://community.nxp.com/docs/DOC-332187"
2. make imx_v7_mfg_defconfig
2. make
3. bitbake fsl-image-manufacturing
4. mkimage -A arm -O linux -T ramdisk -a 0x12c00000 -n "initramfs" -d fsl-image-manufacturing-imx6slevk.cpio.gz initramfs.cpio.gz.uboot
5. changed initramfs.cpio.gz.boot
6. Download firmware by mfgtool but still failed.
The modified code(mmc.c) does not seem to be reflected because I added the log but it is not visible.
)