MCUXpresso v11.5 lvgl examples is not response.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso v11.5 lvgl examples is not response.

732件の閲覧回数
sukyeong
Contributor III

First of all i am using the EVK MIMXRT1160 and LCD.
There is no response when debugging after inserting an example using 'import SDK example'.
When I simulated using the GUI Guider Version 1.3, it is displayed well on the LCD.

Compiler is MCUXpresso v11.5

Is there something I'm missing out on?

0 件の賞賛
返信
1 返信

726件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Actually, I'm not very clear with your question, whether you mean that you fail to debug the LVGL demos from the SDK library for the MIMXRT1160-EVK.
Is my understanding right? If yes, can you tell me the version of the SDK library you used?

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信