Hi,
Is MCUEXPRESSO Ide supports for the IMX8M MINI EVK board, if it supports can you share the SDK for Linux OS and the procedure for building, using the boards.
Hi Vinith
yes i.MX8M Mini EVK is supported, it can be built on below link
https://mcuxpresso.nxp.com/en/welcome
Best regards
igor
After selecting the exact processor there are two files and which I need to choose
1.select Development Board:
2. select EVK-MIMX8MM(MIMX8MM6XXXLZ)
3. Build
I was able to download the sdk when i was dragging the zip file into the installed sdk it throwing the above error