MCP2518fd operation not supported

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCP2518fd operation not supported

736 Views
tzeng015
Contributor II

Hi all

My Board : imx8mm

Linux OS : 5.10

I used the MCP2518fd in our system and the driver is ported ok. I want to test the lookback function and it can't work well. 

This is my commend

ip link set up can0 type can bitrate 500000 restart-ms 6000 fd off loopback on

Please see the attach file and the lookback on function doesn't support

Can you help me ?

thank you

tzeng015

 

 

0 Kudos
Reply
1 Reply

722 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

this is for MX8MM? it does not have CAN interface, if it for MPC51xx please create a thread in tha forum of MPC51XX .

 

Regards

0 Kudos
Reply