MCLK from GPIO_0 or any other GPIO.?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCLK from GPIO_0 or any other GPIO.?

Jump to solution
886 Views
prev
Contributor II

I want to generate MCLK for Audio Codec section.

From Sabre Evaluation board, CSI_MCLK is generated from GPIO_0,

My understanding is that CCM clock can be generated from the below pins of GPIO_0, GPIO_5, GPO_19.

Can we generate the same MCLK from any other GPIO ? or we need to use only these.

pastedImage_0.png

Please clarify me

Thanks

M. Prev Ravanth

Labels (1)
Tags (2)
0 Kudos
1 Solution
690 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prev

no, from any other GPIOs it is not possible to generate clock.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
691 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prev

no, from any other GPIOs it is not possible to generate clock.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
690 Views
prev
Contributor II

Hi Igor,

Can i use  NANDF_CS2 for clock generation of Audio MCLK

pastedImage_0.png

Thanks

M. Prev Ravanth

0 Kudos