According to AN12195, I use the lp_record application to record, but the microphone input of the audio jack on the evaluation board is connected to GND.What path are you using to record?
The i.MX8M needs to be connected to the J1801 connector trough a ribbon cable. With this you will be able to connect SAI ports to other codecs to play/record audio.
Best regards.
Hi Jorge7u7,
In the AN12195 application note sample application, is the audio output through J1801?
The IAR project (audio server) for Cortex-M4 has a WM8524 codec driver, I thought it would be output from the audio jack, is it a difference in my perception?
Also, what kind of audio devices can be connected to the J1801?
Best regards.
Hi Jorge,
Which file is the attached file?
Best regards.
Apologies, I did not upload the file.
I updated the last reply with the corresponding file.
Best regards.