MCIMX8M-EVK not able to Boot from SD Card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX8M-EVK not able to Boot from SD Card

ソリューションへジャンプ
2,578件の閲覧回数
azhar
Contributor III

Hello folks.

I have a new MCIMX8M-EVK. It came with Android pre-installed. I would like to have Linux installed. I looked as quick start guide : Get Started with the MCIMX8M-EVK | NXP Semiconductors

I tried to flash a new sd-card under windows (using mfgtool). I wasn't able to do because mfgtool could not find the device (board). The version : 
L4.9.88_2.0.0_mfg-tool\L4.9.88_2.0.0_mfg-tool\mfgtools-with-rootfs\mfgtools\mfgtool2-yocto-mx-evk-sdcard-sd2.vbs
In this case it appeared that when I change SW802 to 01 the device doesn't boot. No output on the console.

Then I flashed the sd-card on linux and it went well. The pre-built image is: 
fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard

But when I put the sd-card and switched SW802 to 10 and SW801 to 1100 the device doesn't boot. No output on the console. In fact I tried all possible combinations (16) for SW801 nothing worked.

It still boots to pre-installed Android with SW802 to 10 and SW801 to 0010 (eMMC).

Let me know how can I resolve this?

I am open to the idea of flashing the eMMC as well. But don't know how in this scenario?

PS: I already looked at : i.MX Linux® User's Guide (nxp.com).  

 

0 件の賞賛
返信
1 解決策
2,556件の閲覧回数
azhar
Contributor III

Hi Israel.

No, it is still booting from sdcard but with switch setting of eMMC (SW801 to 0010). Strange.
Is this expected behavior?
 
Azhar

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,562件の閲覧回数
azhar
Contributor III

Hi Israel.

Thanks for the prompt response. The flashing with uuu went fine (windows 10). But board refuses to boot after I put SW802 to 10.

Regards.

Azhar

0 件の賞賛
返信
2,566件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi Azhar,

 

I will try to put a step-by-step guide:

So first I recommend flashing the image that we have on our web page, For this, I select the latest release, https://www.nxp.com/webapp/Download?colCode=L5.10.9_1.0.0_MX8MQ&appType=license, so please download it.

Second, It will depend on what system you will work (Linux or Windows), So from the image that you downloaded will have an uuu.auto file that will flash automatically on the memory that is selected with the switches, with that on windows use this: uuu .\uuu.auto

To flash with the UUU tool you need to have the executable from the tool on the same folder that you have the images you want to flash, you can download the tool from the next page: https://github.com/NXPmicro/mfgtools/releases/tag/uuu_1.4.72

Install a serial console viewer, just as the quick guide said (https://www.nxp.com/document/guide/get-started-with-the-mcimx8m-evk:GS-MCIMX8M-EVK#title2.2.2), be sure that you open the correct debug terminal, usually when you connect the i.MX board will add 4 new ports, so I recommend opening all of them just to know which one is for the cortex A53, commonly is the latest but try as I said before.

Then on the board select the correct configuration SW, first the SW802 select the serial downloader mode:
BOOT_MODE 0 => 0
BOOT_MODE 1 => 1

and the next SW801 will depend on what you have selected, eMMC or the SD,
Boot from EMMC => 0010
Boot from SD2 => 1100

You can find this info also on the i.MX 8M EVK Board Hardware User's Guide: https://www.nxp.com/webapp/Download?colCode=IMX8MEVKBHUG

On the board connect to the USB debug port and the USB type C to the computer. When the flash starts you will see activity on one of the serial consoles that are the signal of activity, after the uuu finish flashing the board, move the SW802 to internal boot and it will boot your system.

 

Hope this helps you.

Regards,

Israel.

0 件の賞賛
返信
2,558件の閲覧回数
azhar
Contributor III

Hi Isreal.

It appears that when I tried to flash sdcard (with SW801 to 1100) earlier, it in fact, flashed the eMMC. Now Android is removed from eMMC. So, it seems that, the SW801 switches are malfunctioning. Now when I set SW801 to 0010 it boots to linux.

Azhar

0 件の賞賛
返信
2,555件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Well it nice to hear that now you can boot Linux, and one thing that you can do if the SW are working is checking if you see transition when you move this.

0 件の賞賛
返信
2,557件の閲覧回数
azhar
Contributor III

Hi Israel.

No, it is still booting from sdcard but with switch setting of eMMC (SW801 to 0010). Strange.
Is this expected behavior?
 
Azhar
0 件の賞賛
返信