MCIMX7D5EVM10SD vs MCIMX7D5EVM10SC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX7D5EVM10SD vs MCIMX7D5EVM10SC

ソリューションへジャンプ
1,521件の閲覧回数
yevgeniy_maksim
Contributor I

Hello,

I have been using MCIMX7D5EVM10SD for our product development for some time now, which is a 1.3 silicon version.  My question is how "safe" is it to go back to 1.2 silicon version?  I understand it is not recommended, but what kind of system performance changes am I looking into?  Are there any known problem I will inherent going back to MCIMX7D5EVM10SC (besides discontinued part)?  I checked the errata list for both of the versions and they look very similar.  The diffs are the following:

D (1.3 version): e11166,

C (1.2 version): e10728, e10787, e10629

Thanks,

Yevgeniy

ラベル(1)
0 件の賞賛
返信
1 解決策
1,517件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

There is no performance change, we have security issue located in the rev 1.2 which has been fixed in the rev 1.3 and this is explain in the erratum e11166 takes place only for the i.MX7 Silicon Revision 1.3, where the boot ROM  vulnerability fixes were applied. In this sense e11166 may be considered as result of the ROM fixes

As for security vulnerability errata ERR010872 and ERR010873 (rev 1.2) - please use the following resource.

i.MX & Vybrid Security Vulnerability Errata - ERR010872, ERR010873”

  https://community.nxp.com/docs/DOC-334996

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,518件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

There is no performance change, we have security issue located in the rev 1.2 which has been fixed in the rev 1.3 and this is explain in the erratum e11166 takes place only for the i.MX7 Silicon Revision 1.3, where the boot ROM  vulnerability fixes were applied. In this sense e11166 may be considered as result of the ROM fixes

As for security vulnerability errata ERR010872 and ERR010873 (rev 1.2) - please use the following resource.

i.MX & Vybrid Security Vulnerability Errata - ERR010872, ERR010873”

  https://community.nxp.com/docs/DOC-334996

 

 

 

0 件の賞賛
返信
1,514件の閲覧回数
yevgeniy_maksim
Contributor I

Thanks a lot!

0 件の賞賛
返信