MCIMX7D5EVM10SD vs MCIMX7D5EVM10SC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCIMX7D5EVM10SD vs MCIMX7D5EVM10SC

跳至解决方案
1,523 次查看
yevgeniy_maksim
Contributor I

Hello,

I have been using MCIMX7D5EVM10SD for our product development for some time now, which is a 1.3 silicon version.  My question is how "safe" is it to go back to 1.2 silicon version?  I understand it is not recommended, but what kind of system performance changes am I looking into?  Are there any known problem I will inherent going back to MCIMX7D5EVM10SC (besides discontinued part)?  I checked the errata list for both of the versions and they look very similar.  The diffs are the following:

D (1.3 version): e11166,

C (1.2 version): e10728, e10787, e10629

Thanks,

Yevgeniy

标签 (1)
0 项奖励
回复
1 解答
1,519 次查看
jamesbone
NXP TechSupport
NXP TechSupport

There is no performance change, we have security issue located in the rev 1.2 which has been fixed in the rev 1.3 and this is explain in the erratum e11166 takes place only for the i.MX7 Silicon Revision 1.3, where the boot ROM  vulnerability fixes were applied. In this sense e11166 may be considered as result of the ROM fixes

As for security vulnerability errata ERR010872 and ERR010873 (rev 1.2) - please use the following resource.

i.MX & Vybrid Security Vulnerability Errata - ERR010872, ERR010873”

  https://community.nxp.com/docs/DOC-334996

 

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,520 次查看
jamesbone
NXP TechSupport
NXP TechSupport

There is no performance change, we have security issue located in the rev 1.2 which has been fixed in the rev 1.3 and this is explain in the erratum e11166 takes place only for the i.MX7 Silicon Revision 1.3, where the boot ROM  vulnerability fixes were applied. In this sense e11166 may be considered as result of the ROM fixes

As for security vulnerability errata ERR010872 and ERR010873 (rev 1.2) - please use the following resource.

i.MX & Vybrid Security Vulnerability Errata - ERR010872, ERR010873”

  https://community.nxp.com/docs/DOC-334996

 

 

 

0 项奖励
回复
1,516 次查看
yevgeniy_maksim
Contributor I

Thanks a lot!

0 项奖励
回复