MCIMX7D5EVM10SD is it a direct substitute for MCIMX7D5EVM10SC

cancel
Showing results for 
Search instead for 
Did you mean: 

MCIMX7D5EVM10SD is it a direct substitute for MCIMX7D5EVM10SC

251 Views
talents_titus
Contributor I

I'm currently using i.MX 7Dual for a design. The requirement specifies industrial grade components. My question is MCIMX7D5EVM10SD a direct substitute for MCIMX7D5EVM10SC. The confusion is due to the comparison table in the Buy/Parameter section of NXP which defines MCIMX7D5EVM10SD as  Heterogeneous Processing with dual Arm® Cortex®. Can I used it instead of MCIMX7D5EVM10SC? Thanks 

Labels (1)
0 Kudos
2 Replies

135 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Talents Titus,

The MCIMX7D5EVM10SD (Silicon Revision 1.3) is a direct replacement for the MCIMX7D5EVM10SC (Silicon Revision 1.2). You can see the part number nomenclature on Figure 1 of the i.MX7D Datasheet (link below)

https://www.nxp.com/docs/en/data-sheet/IMX7DCEC.pdf

Al i.M7 processors are heterogeneous because of the addition of a smaller Cortex-M4 core in ad

dition to the main Cortex-A7 core(s). My apologies for the confusion from the description on the comparison table.

Regards,

0 Kudos

135 Views
talents_titus
Contributor I

Thanks so much for the help. 

0 Kudos