MCIMX6Y2CVM08AB的问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6Y2CVM08AB的问题

Jump to solution
1,420 Views
longbin
Contributor II

因为MCIMX6Y2CVM05AB要更换为MCIMX6Y2CVM08AB。

问题一:内核改成4.1.15_2.1.0,我现在的内核是4.1.15_2.0.1.我现在修改linux-imx-4.1.15.bb。修改如下:

2BF59503-AE65-4389-B92F-0DA46FB03EA5.png

结果编译出错:

76F8D8FB-70F4-4d1d-AD69-B488A23836EF.png

git://git.freescale.com/imx/linux-imx.git应该改成什么???

问题二:ddr_stress_tester_v3.00内的imx6ull的ARM Speed没有800MHz,应该怎么做??用700MHz是否可行?

Labels (1)
0 Kudos
1 Solution
1,085 Views
joanxie
NXP TechSupport
NXP TechSupport

why don't you just use this command directly?

"repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-4.1-krogoth -m imx-4.1.15-2.0.0.xml"

View solution in original post

0 Kudos
6 Replies
1,085 Views
joanxie
NXP TechSupport
NXP TechSupport

1) try to change the ""git://git.freescale.com/imx" " to "https://source.codeaurora.org/external/imx"

2)you can set it as default

0 Kudos
1,085 Views
longbin
Contributor II

非常感谢您的帮忙。

我把 ""git://git.freescale.com/imx/linux-imx.git" " to git://codeaurora.org/external/imx/linux-imx.git。并且去掉

SRC_URI +=

"file://0001-ARM-imx-imx6ul-add-PHY-KSZ8081-new-silicon-revision-.pa#tch \      

file://0001-MLK-13418-ASoC-wm8960-workaround-no-sound-issue-in-m.pat#ch \        

file://0002-MLK-13422-ASoC-wm8960-fix-the-pitch-shift-issue-afte.pat#ch "

可以编译正确,但是 DISTRO_VERSION   = "4.1.15-2.0.1"。而不是4.1.15-2.1.0 我担心有问题。

然后我就git clone https://source.codeaurora.org/external/imx/meta-fsl-bsp-release -b nxp/krogoth_4.1.15-2.0.0_patch,替换掉以前的meta-fsl-bsp-release。这样DISTRO_VERSION   = "4.1.15-2.0.3"。我这样做是否可以???

0 Kudos
1,086 Views
joanxie
NXP TechSupport
NXP TechSupport

why don't you just use this command directly?

"repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-4.1-krogoth -m imx-4.1.15-2.0.0.xml"

0 Kudos
1,085 Views
longbin
Contributor II

非常感谢,今天我已经这样做了:"repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-4.1-krogoth,没有加 -m imx4.1.15-2.0.0.xml,不加-m imx4.1.15-2.0.0.xml有没有问题?我对yocto以及git不熟悉,我开始只想升级linux-imx.bb,编译出错后,我就想到改成层,然后想到以后不能自动升级,才想到这样做。

0 Kudos
1,085 Views
joanxie
NXP TechSupport
NXP TechSupport

if you want to change 4.1.15_2.0.1 to 4.1.15_2.1.0, pls add "-m "

0 Kudos
1,085 Views
longbin
Contributor II

非常感谢。因为对yocto不熟悉,怕改错了,所以重新创建,也就没有加。

0 Kudos