因为MCIMX6Y2CVM05AB要更换为MCIMX6Y2CVM08AB。
问题一:内核改成4.1.15_2.1.0,我现在的内核是4.1.15_2.0.1.我现在修改linux-imx-4.1.15.bb。修改如下:
结果编译出错:
git://git.freescale.com/imx/linux-imx.git应该改成什么???
问题二:ddr_stress_tester_v3.00内的imx6ull的ARM Speed没有800MHz,应该怎么做??用700MHz是否可行?
Solved! Go to Solution.
why don't you just use this command directly?
"repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-4.1-krogoth -m imx-4.1.15-2.0.0.xml"
1) try to change the ""git://git.freescale.com/imx" " to "https://source.codeaurora.org/external/imx"
2)you can set it as default
非常感谢您的帮忙。
我把 ""git://git.freescale.com/imx/linux-imx.git" " to git://codeaurora.org/external/imx/linux-imx.git。并且去掉
SRC_URI +=
"file://0001-ARM-imx-imx6ul-add-PHY-KSZ8081-new-silicon-revision-.pa#tch \
file://0001-MLK-13418-ASoC-wm8960-workaround-no-sound-issue-in-m.pat#ch \
file://0002-MLK-13422-ASoC-wm8960-fix-the-pitch-shift-issue-afte.pat#ch "
可以编译正确,但是 DISTRO_VERSION = "4.1.15-2.0.1"。而不是4.1.15-2.1.0 我担心有问题。
然后我就git clone https://source.codeaurora.org/external/imx/meta-fsl-bsp-release -b nxp/krogoth_4.1.15-2.0.0_patch,替换掉以前的meta-fsl-bsp-release。这样DISTRO_VERSION = "4.1.15-2.0.3"。我这样做是否可以???
why don't you just use this command directly?
"repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-4.1-krogoth -m imx-4.1.15-2.0.0.xml"
非常感谢,今天我已经这样做了:"repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b imx-4.1-krogoth,没有加 -m imx4.1.15-2.0.0.xml,不加-m imx4.1.15-2.0.0.xml有没有问题?我对yocto以及git不熟悉,我开始只想升级linux-imx.bb,编译出错后,我就想到改成层,然后想到以后不能自动升级,才想到这样做。
if you want to change 4.1.15_2.0.1 to 4.1.15_2.1.0, pls add "-m "
非常感谢。因为对yocto不熟悉,怕改错了,所以重新创建,也就没有加。