MCIMX6Y2CVM08AA processor - VDDA_ADC_3P3 pin voltage is 3.9V without the power input to this particular voltage input pin L13 (VDDA_ADC_3P3)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6Y2CVM08AA processor - VDDA_ADC_3P3 pin voltage is 3.9V without the power input to this particular voltage input pin L13 (VDDA_ADC_3P3)

896 Views
jayebc
Contributor II

Hi,

On the custom hardware we are using MCIMX6Y2CVM08AA processor. After power ON, all the voltage levels are fine except the VDDA_ADC_3P3 which is 3.9V so i remove the power input to this particular voltage input pin L13 (VDDA_ADC_3P3) but still see a voltage level of 3.9V on this pin (without power connected to this particular pin).

Can you please suggest us any debugging steps or a solution if this is a known issue.

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

513 Views
Yuri
NXP Employee
NXP Employee

 

Hello,

 

   verify Your design, if it meets the  Hardware Development Guide :

https://www.nxp.com/docs/en/user-guide/IMX6ULLHDG.pdf 

 

  Also use

https://community.nxp.com/docs/DOC-129659 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply