MCIMX6ULL LCD touch calibration not preserved

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX6ULL LCD touch calibration not preserved

625件の閲覧回数
whizpb
Contributor I

I am using iMX6ULL EVK with LCD8000-43T which is a compatible LCD provided with the EVK. 

On boot up, the LCD asks for touch calibration. Once this calibration is done and reboot the kit, the calibration is again asked for. Does the BSP not allow preserving the LCD touch calibration once it is done?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

535件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the linux BSP ? About the BSP Supported Features you can see the i.MX_Linux_Release_Notes.pdf.

0 件の賞賛
返信

535件の閲覧回数
whizpb
Contributor I

Yes, I am using Linux BSP. I could not find anything specific to LCD calibration support in i.MX_Linux_Release_Notes.pdf.

0 件の賞賛
返信