MCIMX6ULL-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6ULL-EVK

1,722 Views
m-lapalus
Contributor I

Dear All,

Do someone have the board in .ALG file (ASCII Allegro) to import with Altium Designer ?

Many thanks

Michel

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

1,646 Views
Rodrigue
NXP Employee
NXP Employee

Hi Yuri,

May you please send them to me as well?

 

best regards,

 

Rod

0 Kudos
Reply

1,550 Views
berndfischer
Contributor I

Hi Rod

 

could you share the ALG files for the EVK with me as well please? If you got them.  I have a customer that also asked for them.  

 

Regards

Bernd 

EBV Electronik

0 Kudos
Reply

1,650 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

 I've sent You files directly. 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply

1,476 Views
Lalitkumarbaghel
Contributor I

Hi @Yuri

I am trying to develop BLE gateway based on MCIMX6ULL-EVK.

Please send me the Altium Files for Base board and Carrier Board of MCIMX6ULL-EVK kit.

 

0 Kudos
Reply

1,461 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply