I am also intresed in PF0100 inductor currents. Are there peak switching current values avalible or load line figures for the high current loops of the switchers? If this data is published in one of the application notes could you point me in the right direction.
As for power consumption estimations, please use the AN4580 :
"i.MX 6SoloLite Power Consumption Measurement"
http://cache.freescale.com/files/32bit/doc/app_note/AN4580.pdf
Also, i.MX6 Datasheets contain sections "Maximum Supply Currents"
and "Low Power Mode Supply Currents".
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SLCEC.pdf
As for PF0100 inductor currents, please refer to PF0100 Datasheet.
Summary Page :
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MMPF0100