MCIMX6L2EVN10, typical power (min, max, surge) for the power rails? Do you have numbers for EVK (MCIMX6SLEVK board)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6L2EVN10, typical power (min, max, surge) for the power rails? Do you have numbers for EVK (MCIMX6SLEVK board)?

520 Views
RobertCorrellus
Contributor II

I am also intresed in PF0100 inductor currents.  Are there peak switching current values avalible or load line figures for the high current loops of the switchers?  If this data is published in one of the application notes could you point me in the right direction.

Labels (2)
Tags (3)
0 Kudos
1 Reply

394 Views
Yuri
NXP Employee
NXP Employee

As for power consumption estimations, please use the AN4580 :

"i.MX 6SoloLite Power Consumption Measurement"

http://cache.freescale.com/files/32bit/doc/app_note/AN4580.pdf

Also, i.MX6 Datasheets contain  sections "Maximum Supply Currents"

and "Low Power Mode Supply Currents".

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SLCEC.pdf 


As for PF0100 inductor currents, please refer to PF0100 Datasheet.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MMPF0100&tab=Documentation_Tab&pspll=...

Summary Page :

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MMPF0100

0 Kudos