MCIMX6DLAICPU2 - 5.10.72 - apt-get update not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6DLAICPU2 - 5.10.72 - apt-get update not working

2,664 Views
B_Prabhu
Contributor III

I can't able to install new package so tried to update package index files on the system by using apt-get update, getting below error.

Can you pls support to resolve this?

Logfile:

Get:1 http://ftp.debian.org/debian buster InRelease [122 kB]
Get:2 http://ftp.debian.org/debian buster-updates InRelease [51.9 kB]
Err:1 http://ftp.debian.org/debian buster InRelease
gpgv, gpgv2 or gpgv1 required for verification, but neither seems installed
Err:2 http://ftp.debian.org/debian buster-updates InRelease
gpgv, gpgv2 or gpgv1 required for verification, but neither seems installed
Reading package lists... Done
W: GPG error: http://ftp.debian.org/debian buster InRelease: gpgv, gpgv2 or gpgv1 required for verification, but neither seems installed
E: The repository 'http://ftp.debian.org/debian buster InRelease' is not signed.
N: Updating from such a repository can't be done securely, and is therefore disabled by default.
N: See apt-secure(8) manpage for repository creation and user configuration details.
W: GPG error: http://ftp.debian.org/debian buster-updates InRelease: gpgv, gpgv2 or gpgv1 required for verification, but neither seems installed
E: The repository 'http://ftp.debian.org/debian buster-updates InRelease' is not signed.
N: Updating from such a repository can't be done securely, and is therefore disabled by default.
N: See apt-secure(8) manpage for repository creation and user configuration details.

0 Kudos
Reply
6 Replies

2,652 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @B_Prabhu 

Regarding this issue, I have confirmed with internal experts that debian-10.list is only for demonstrating support for APT install, but debian 10 repo has strengthened security certification. It is recommended to build a package repo on the intranet, and then create sources.list.

 

Best regards

Harvey

0 Kudos
Reply

2,626 Views
B_Prabhu
Contributor III

Hi Harvey,

Thanks for the feedback.

I have checked in the GitHub the latest version is below.

https://github.com/nxp-imx/imx-manifest -b imx-linux-langdale -m imx-6.1.1-1.0.0.xml

https://github.com/nxp-imx/imx-manifest

I need support from you, can you pls share the build image for this so that i can directly flash in my board. When i am trying to download this file i got some error i can't able to download also i am not sure about this build process because i am new to this topic.

If you share the build image it would be great help for me..

0 Kudos
Reply

2,617 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

Probably temporarily network issue, you can try to download it at another time: Prebuilt image for all available SoC and BSP at (Embedded Linux for i.MX Applications Processors | NXP Semiconductors). 

This document provides more details for build process for your reference: i.MX Yocto Project User's Guide (nxp.com)

 

Best regards

Harvey

0 Kudos
Reply

2,608 Views
B_Prabhu
Contributor III

Hi Harvey,

Already i build the 5.10.72.2.2.3 image there only i got below error (which i explained in first post).

Can you share the build image from GitHub it would be great help for me.

0 Kudos
Reply

2,578 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

We don't provide build image from Github, as said, you can find all available from Embedded Linux for i.MX Applications Processors | NXP Semiconductors

and I just tried to download one there is no problem for downloading. 

 

Best regards

Harvey

0 Kudos
Reply

2,528 Views
B_Prabhu
Contributor III

Hi, 

I have started building the image from GitHub -  https://github.com/nxp-imx/imx-manifest/tree/imx-linux-hardknott

Followed step by step procedure from the same link and i build the yocto project successfully but i didn't see the .sdcard or .wic file in the tmp/deploy/image. Is there any further process do i need to follow to get those files.

0 Kudos
Reply