MCIMX6DLAICPU2 - 5.10.72 - apt-get update not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX6DLAICPU2 - 5.10.72 - apt-get update not working

2,460件の閲覧回数
B_Prabhu
Contributor III

I can't able to install new package so tried to update package index files on the system by using apt-get update, getting below error.

Can you pls support to resolve this?

Logfile:

Get:1 http://ftp.debian.org/debian buster InRelease [122 kB]
Get:2 http://ftp.debian.org/debian buster-updates InRelease [51.9 kB]
Err:1 http://ftp.debian.org/debian buster InRelease
gpgv, gpgv2 or gpgv1 required for verification, but neither seems installed
Err:2 http://ftp.debian.org/debian buster-updates InRelease
gpgv, gpgv2 or gpgv1 required for verification, but neither seems installed
Reading package lists... Done
W: GPG error: http://ftp.debian.org/debian buster InRelease: gpgv, gpgv2 or gpgv1 required for verification, but neither seems installed
E: The repository 'http://ftp.debian.org/debian buster InRelease' is not signed.
N: Updating from such a repository can't be done securely, and is therefore disabled by default.
N: See apt-secure(8) manpage for repository creation and user configuration details.
W: GPG error: http://ftp.debian.org/debian buster-updates InRelease: gpgv, gpgv2 or gpgv1 required for verification, but neither seems installed
E: The repository 'http://ftp.debian.org/debian buster-updates InRelease' is not signed.
N: Updating from such a repository can't be done securely, and is therefore disabled by default.
N: See apt-secure(8) manpage for repository creation and user configuration details.

0 件の賞賛
返信
6 返答(返信)

2,448件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi @B_Prabhu 

Regarding this issue, I have confirmed with internal experts that debian-10.list is only for demonstrating support for APT install, but debian 10 repo has strengthened security certification. It is recommended to build a package repo on the intranet, and then create sources.list.

 

Best regards

Harvey

0 件の賞賛
返信

2,422件の閲覧回数
B_Prabhu
Contributor III

Hi Harvey,

Thanks for the feedback.

I have checked in the GitHub the latest version is below.

https://github.com/nxp-imx/imx-manifest -b imx-linux-langdale -m imx-6.1.1-1.0.0.xml

https://github.com/nxp-imx/imx-manifest

I need support from you, can you pls share the build image for this so that i can directly flash in my board. When i am trying to download this file i got some error i can't able to download also i am not sure about this build process because i am new to this topic.

If you share the build image it would be great help for me..

0 件の賞賛
返信

2,413件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

Probably temporarily network issue, you can try to download it at another time: Prebuilt image for all available SoC and BSP at (Embedded Linux for i.MX Applications Processors | NXP Semiconductors). 

This document provides more details for build process for your reference: i.MX Yocto Project User's Guide (nxp.com)

 

Best regards

Harvey

0 件の賞賛
返信

2,404件の閲覧回数
B_Prabhu
Contributor III

Hi Harvey,

Already i build the 5.10.72.2.2.3 image there only i got below error (which i explained in first post).

Can you share the build image from GitHub it would be great help for me.

0 件の賞賛
返信

2,374件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

We don't provide build image from Github, as said, you can find all available from Embedded Linux for i.MX Applications Processors | NXP Semiconductors

and I just tried to download one there is no problem for downloading. 

 

Best regards

Harvey

0 件の賞賛
返信

2,324件の閲覧回数
B_Prabhu
Contributor III

Hi, 

I have started building the image from GitHub -  https://github.com/nxp-imx/imx-manifest/tree/imx-linux-hardknott

Followed step by step procedure from the same link and i build the yocto project successfully but i didn't see the .sdcard or .wic file in the tmp/deploy/image. Is there any further process do i need to follow to get those files.

0 件の賞賛
返信