MCIMX6DL-SDP SCH-27417 REV B3 RUN L3.0.35_4.0.0_130424 Linux and android_jb4.2.2_1.0.0 kernel crash, the other Rev. Linux and Android4.0.4 work well,
if the newest version linux and android 4.2.2 not support on old version MX6D/DL-SDP/B Borad? Thanks
U-Boot 2009.08 (Apr 25 2013 - 01:36:51)
CPU: Freescale i.MX6 family TO1.0 at 792 MHz
Temperature: can't get valid data!
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 198000000Hz
emi_slow clock: 99000000Hz
ddr clock : 396000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6DL/Solo-SABRESD: RevC Board: 0x61310 [POR ]
Boot Device: MMC
I2C: ready
DRAM: 1 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3
In: serial
Out: serial
Err: serial
i2c: I2C3 SDA is low, start i2c recovery...
I2C3 Recovery success
Found PFUZE100! deviceid=10,revid=10
Net: got MAC address from IIM: 00:04:9f:02:30:f1
FEC0 [PRIME]
Hit any key to stop autoboot: 0
mmc3(part 0) is current device
MMC read: dev # 3, block # 2048, count 8192 ... 8192 blocks read: OK
## Booting kernel from Legacy Image at 10800000 ...
Image Name: Linux-3.0.35-2508-g54750ff
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3860964 Bytes = 3.7 MB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 3.0.35-2508-g54750ff (lucid@ubuntu) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #3 SMP PREEMPT Tue Jun 25 18:42:30 PDT 2013
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board
Ignoring unrecognised tag 0x54410008
Memory policy: ECC disabled, Data cache writealloc
CPU identified as i.MX6DL/SOLO, silicon rev 1.0
PERCPU: Embedded 7 pages/cpu @8c008000 s5440 r8192 d15040 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 227328
Kernel command line: console=ttymxc0,115200 ip=dhcp root=/dev/mmcblk0p1 rootwait
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 640MB 256MB = 896MB total
Memory: 896908k/896908k available, 151668k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xf4600000 - 0xffe00000 ( 184 MB)
vmalloc : 0xc0800000 - 0xf2000000 ( 792 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.init : 0x80008000 - 0x8003b000 ( 204 kB)
.text : 0x8003b000 - 0x80a8d874 (10571 kB)
.data : 0x80a8e000 - 0x80af1c00 ( 399 kB)
.bss : 0x80af1c24 - 0x80b3fb4c ( 312 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:624
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
Set periph_clk's parent to pll2_pfd_400M!
arm_max_freq=800MHz
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole [ttymxc0] enabled
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
CPU1: Booted secondary processor
Brought up 2 CPUs
SMP: Total of 2 processors activated (3162.11 BogoMIPS).
print_constraints: dummy:
NET: Registered protocol family 16
print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal
print_constraints: vddcore: 725 <--> 1300 mV at 1100 mV fast normal
print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal
print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x02050000, Cache size: 524288 B
bio: create slab <bio-0> at 0
mxs-dma mxs-dma-apbh: initialized
print_constraints: SPKVDD: 4200 mV
print_constraints: vmmc: 3300 mV
SCSI subsystem initialized
spi_imx imx6q-ecspi.0: probed
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Freescale USB OTG Driver loaded, $Revision: 1.55 $
mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 0
mc_pfuze 1-0008: FAB: 0 ,FIN: 0
PF100 1.0 chip found!
print_constraints: PFUZE100_SW1A: 300 <--> 1875 mV at 1300 mV
print_constraints: PFUZE100_SW1B: 300 <--> 1875 mV at 300 mV
print_constraints: PFUZE100_SW1C: 300 <--> 1875 mV at 1300 mV
print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3300 mV
print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1500 mV
print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1500 mV
print_constraints: PFUZE100_SW4: 800 <--> 3950 mV at 3150 mV
print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV
print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 3000 mV
print_constraints: PFUZE100_VREFDDR: at 750 mV
print_constraints: PFUZE100_VGEN1: 800 <--> 1550 mV at 1500 mV
print_constraints: PFUZE100_VGEN2: 800 <--> 1550 mV at 1500 mV
print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 2800 mV
print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV
print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 3000 mV
print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 3300 mV
imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Version 1.0.24.
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
cfg80211: Calling CRDA to update world regulatory domain
max17135 2-0048: PMIC MAX17135 for eInk display
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
TCP: Hash tables configured (established 131072 bind 65536)
TCP reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
PMU: registered new PMU device of type 0
Static Power Management for Freescale i.MX6
wait mode is enabled for i.MX6
cpaddr = c0820000 suspend_iram_base=c08bc000
PM driver module loaded
IMX usb wakeup probe
add wake up source irq 75
IMX usb wakeup probe
cpu regulator mode:ldo_bypass
_regulator_get: get() with no identifier
mx6_cpu_regulator_init: failed to get pu regulator
i.MXC CPU frequency driver
JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
msgmni has been set to 1751
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb
_regulator_get: get() with no identifier
imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 128x48
mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled, bootconsole disabled
console [ttymxc0] enabled, bootconsole disabled
loop: module loaded
m25p80 spi0.0: found m25p32, expected sst25vf016b
m25p80 spi0.0: m25p32 (4096 Kbytes)
Creating 2 MTD partitions on "m25p80":
0x000000000000-0x000000100000 : "bootloader"
0x000000100000-0x000000400000 : "kernel"
GPMI NAND driver registered. (IMX)
vcan: Virtual CAN interface driver
CAN device driver interface
flexcan netdevice driver
FEC Ethernet Driver
fec_enet_mii_bus: probed
Internal error: Oops - undefined instruction: 0 [#1] PREEMPT SMP
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00100000
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00800000
Modules linked in:
CPU: 1 Not tainted (3.0.35-2508-g54750ff #3)
PC is at check_unsafe_exec+0xa0/0xec
LR is at check_unsafe_exec+0x4c/0xec
pc : [<800f7058>] lr : [<800f7004>] psr: 60000013
sp : bfc41f30 ip : 00000004 fp : 00000000
r10: bfc41f78 r9 : 00000000 r8 : bffb0000
r7 : 00000000 r6 : 00000001 r5 : bffb0000 r4 : 00000000
r3 : bfd3a0a0 r2 : 00000001 r1 : 00000000 r0 : 00000000
Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 10c53c7d Table: 1000404a DAC: 00000015
Process kworker/u:0 (pid: 1269, stack limit = 0xbfc402f0)
Stack: (0xbfc41f30 to 0xbfc42000)
1f20: bfc40000 bfd3a204 80ac9ee0 bff8be3c
1f40: bffed000 800f7104 00000000 00000000 bfd395c0 bff8be3c 80ac9ee0 bfc41f78
1f60: bffed000 00000000 00000000 00000000 00000000 800440b0 00000000 00000000
1f80: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
1fa0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
1fc0: ffffffff bfe97980 bfda9120 00000000 ffffffff 00000000 00000000 80087250
1fe0: 00000000 bfe97980 80087154 80041aa4 00000013 80041aa4 7567613f 5ffeed3f
[<800f7058>] (check_unsafe_exec+0xa0/0xec) from [<800f7104>] (do_execve+0x60/0x268)
[<800f7104>] (do_execve+0x60/0x268) from [<800440b0>] (kernel_execve+0x38/0x7c)
[<800440b0>] (kernel_execve+0x38/0x7c) from [<80087250>] (____call_usermodehelper+0xfc/0x124)
[<80087250>] (____call_usermodehelper+0xfc/0x124) from [<80041aa4>] (kernel_thread_exit+0x0/0x8)
Code: bfb66408 bff07060 00000001 000041ed (000032d0)
---[ end trace 834dcbf045cfa199 ]---
note: kworker/u:0[1269] exited with preempt_count 1
Internal error: Oops - undefined instruction: 0 [#2] PREEMPT SMP
Modules linked in:
CPU: 0 Tainted: G D (3.0.35-2508-g54750ff #3)
PC is at check_unsafe_exec+0xa0/0xec
LR is at check_unsafe_exec+0x4c/0xec
pc : [<800f7058>] lr : [<800f7004>] psr: 60000013
sp : ba143f30 ip : 00000004 fp : 00000000
r10: ba143f78 r9 : 00000000 r8 : bfe95100
r7 : 00000000 r6 : 00000001 r5 : bfe95100 r4 : 00000000
r3 : bfd39d00 r2 : 00000001 r1 : 00000000 r0 : 00000000
Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 10c53c7d Table: 1000404a DAC: 00000015
Process kworker/u:0 (pid: 1270, stack limit = 0xba1422f0)
Stack: (0xba143f30 to 0xba144000)
3f20: ba142000 bfd39e64 80ac9ee0 bff8be3c
3f40: bffed000 800f7104 00000000 00000000 bfdb4ae0 bff8be3c 80ac9ee0 ba143f78
3f60: bffed000 00000000 00000000 00000000 00000000 800440b0 00000000 00000000
3f80: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
3fa0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
3fc0: ffffffff bfe97980 bfdc1360 00000000 ffffffff 00000000 00000000 80087250
3fe0: 00000000 bfe97980 80087154 80041aa4 00000013 80041aa4 80203140 00544103
[<800f7058>] (check_unsafe_exec+0xa0/0xec) from [<800f7104>] (do_execve+0x60/0x268)
[<800f7104>] (do_execve+0x60/0x268) from [<800440b0>] (kernel_execve+0x38/0x7c)
[<800440b0>] (kernel_execve+0x38/0x7c) from [<80087250>] (____call_usermodehelper+0xfc/0x124)
[<80087250>] (____call_usermodehelper+0xfc/0x124) from [<80041aa4>] (kernel_thread_exit+0x0/0x8)
Code: bfb66408 bff07060 00000001 000041ed (000032d0)
---[ end trace 834dcbf045cfa19a ]---
note: kworker/u:0[1270] exited with preempt_count 1
已解决! 转到解答。
The new DDR parameters in uboot is tuned for RevC boards, but your board is old RevB board, so I think you can use old version workable UBoot; or replace the "/uboot-imx/board/freescale/mx6q_sabresd/flash_header.S" with the old one.
By the way, "add "enable_wait_mode=off" in the kernel command" is also needed.
It does NOT worked. On the MCIMX6DL-SDP, android 4.2 still can not run stable. Sometimes it can boot into android desktop but after a while, android die and reboot by watchdog; sometimes it can NOT boot into android desktop even.
On the same board, android 4.0 worked well. In our project, we want use android 4.2.
The new DDR parameters in uboot is tuned for RevC boards, but your board is old RevB board, so I think you can use old version workable UBoot; or replace the "/uboot-imx/board/freescale/mx6q_sabresd/flash_header.S" with the old one.
By the way, "add "enable_wait_mode=off" in the kernel command" is also needed.