MCIMX51LCD on imx53 Loco Board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX51LCD on imx53 Loco Board?

1,256 Views
ayc
Contributor I

Hi,

    Does anyone know if the MCIMX51LCD can be used with the imx53 Loco Board?

 

Thanks

Labels (1)
0 Kudos
Reply
4 Replies

1,169 Views
AlanLevy
Contributor I
Yes. It works pretty much out of the box, just use the CLAA-VGA settings. The only problem with it is that the default touchscreen configuration is upside down relative to the display.
0 Kudos
Reply

1,169 Views
ayc
Contributor I
    I meant it plugs into the i.Mx53QSB, but I do not know if the pin-outs are the same (or compatible).

Andy Chang said:

Correct, but we have this MCIMX51LCD left over from the 51EVK and I was wondering if I can use it in the i.mx53QSB and use the LCD code for i.Mx51 in u-boot.

 

It appears to be a fit hardware foot-print wise.

 

0 Kudos
Reply

1,169 Views
ayc
Contributor I

Correct, but we have this MCIMX51LCD left over from the 51EVK and I was wondering if I can use it in the i.mx53QSB and use the LCD code for i.Mx51 in u-boot.

 

It appears to be a fit hardware foot-print wise.

0 Kudos
Reply

1,169 Views
YiLi
Contributor I

Good question, currently MX28LCD is used for i.mx53QSB, which also be used for 28EVK and 50EVK.

 

0 Kudos
Reply