MCF5372, observed distorted output using the model MCF5372LCVM240.ibs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF5372, observed distorted output using the model MCF5372LCVM240.ibs

743 Views
sms2
Contributor I

Hello Everyone,

Request to understand , the reason about the high overshoot/Undershoot, Ripple,Non monotonicity for the Address/Data ,SDRAM,CPU_CLK signal using the model "MCF5372LCVM240.ibs".

pad_rfc_33_01,20pF Drive Strength is the IO used.

FYI,  have replaced the controller and observed  the signal using different controller, the result looks acceptable.

Kindly help me to understand about the model.


0 Kudos
Reply
1 Reply

722 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, I do not see your mentioned overshoot/undershoot situation with attached IBIS file.

Hui_Ma_1-1663895807515.pngHui_Ma_2-1663895832519.png

Mike

0 Kudos
Reply