MC34PF3001A7EP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC34PF3001A7EP

476 Views
shwethanarayan
Contributor I

Hi,

 

Please find the attachment. We are using IMX6 Ultralite processor for one of our project. We have a small query in PMIC PF3001.

 

1. What is the SW1_SEQ, SW2_SEQ and so on?

2. If it is a sequence, then why in A7 series it is mentioned as 3 everywhere.for SW1_SEQ, SW2_SEQ and so on.

3. Do you have EVK with PMIC PF3001 for IMX6 Ultralite?

Please let me know the answers for the above queries.

 

Regards

Shwetha

 

 

0 Kudos
2 Replies

468 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

 See below, please!

------------------------------

1. What is the SW1_SEQ, SW2_SEQ and so on?
It means the sequence of the voltage output.
for example: MC32PF3000A7EP
A7 in the partnumber is configuration , which has it's own output sequence.
See page 35, "Start-up configuration" table.

OTP_SW1A_SEQ----> 3, it means the voltage's output sequence is No.3

2. If it is a sequence, then why in A7 series it is mentioned as 3 everywhere.for SW1_SEQ, SW2_SEQ and so on.
See above, please!

3. Do you have EVK with PMIC PF3001 for IMX6 Ultralite?
Yes, we do.
I will send it to your personal email, check it , please!

--------------------

Have a nice day!

B.R,

Weidong

0 Kudos

465 Views
shwethanarayan
Contributor I

Hi Weidong

 

Thanks for the reply.

 

3. Do you have EVK with PMIC PF3001 for IMX6 Ultralite?
Yes, we do.
I will send it to your personal email, check it , please!

I'm awaiting for your mail on the EVK.

 

Regards

Shwetha

0 Kudos