MC34708 : VSRTC not powerd by the coin cell

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC34708 : VSRTC not powerd by the coin cell

752 Views
jomeke
Contributor II

Hi all,

on one of our boards we are using the iMX537 which is powerd by the PMIC MC34708, on the PMIC there is a 3V coin cell connected.

Until now we produced approximately 1000 unit without any problem.

With the last batch (250 pieces) there are 12 boards with the following failure :

When the power is applied : VSRTC = 1.3V --> OK

When the power is removed : VSRTC drops down to 0V.

So the connected 3V coin cell doesn't take over to feed the VSRTC supply.

We have replaced the PMIC on 3 boards and the problem is solved, so it looks like the PMIC chips are bad....

Has anybody experienced the same problem ?

Could there be an other reason for that behavior ?

Thanks for the respons

Labels (1)
0 Kudos
Reply
1 Reply

657 Views
igorpadykov
NXP Employee
NXP Employee

Hi johan

I had not heard about such issues, but think

that this may be caused by technology process:

solder overheating or ESD handling. In general it may

be recommended to send chips for quality analysis

through marketing local office.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply