MC13892 : different power source domain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC13892 : different power source domain

Jump to solution
1,198 Views
koichisakagami
Contributor II

Dear community,

We consider the MC13892 different power source domains.


In application note AN3867 ( MC13892 Functional Pin Description),
it says that SW1/2/3/4IN and VINUSB2 and VINAUDIO and VINIOHI are connected to BP.

But we hope to connect these pins to the another power source other than the BP.
    The BP is connected to "A power source".
    The SW1/2/3/4IN and VINUSB2 and VINAUDIO and VINIOHI are connected to "B power source".

[Question]
Is the MC13892 equivalent to this use method ?
    If Yes,
        Could you tell us the limit in the use ?
        For example,
            power up sequence related to BP and non-BP power source.
            potential defference value between BP and non-BP power source.

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
Reply
1 Solution
1,117 Views
igorpadykov
NXP Employee
NXP Employee

Hi Koichi

>Is the MC13892 equivalent to this use method ?

Yes.

>If Yes, Could you tell us the limit in the use ?

First should be powered up BP, then non-BP power source.

No special requirements for defference value between BP and

non-BP power source.

Input values of SW1/2/3/4IN and VINUSB2 and VINAUDIO and VINIOHI

should comply with MC13892 datasheet requirements.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,118 Views
igorpadykov
NXP Employee
NXP Employee

Hi Koichi

>Is the MC13892 equivalent to this use method ?

Yes.

>If Yes, Could you tell us the limit in the use ?

First should be powered up BP, then non-BP power source.

No special requirements for defference value between BP and

non-BP power source.

Input values of SW1/2/3/4IN and VINUSB2 and VINAUDIO and VINIOHI

should comply with MC13892 datasheet requirements.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply