Lwip and heap4.c in freertos

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lwip and heap4.c in freertos

ソリューションへジャンプ
508件の閲覧回数
andréluis
Contributor II

Hi, I'm using a MIMXRT1060-EVK. I have an application running lwIP with FreeRTOS, using heap_3. But I need to change my application to run in FreeRTOS with heap_4. When I made the changes, I can build and debug, but I don't even receive a ping. Is there some configuration I need to do to make it work? Thanks for the help.

0 件の賞賛
返信
1 解決策
439件の閲覧回数
Pablo_Ramos
NXP Employee
NXP Employee

Hi,

You can refer to the following community post, in there you will find an explanation of how to switch between heap implementations.

Solved: Re: FreeRTOS, LWIP, MEBDTLS - NXP Community

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
440件の閲覧回数
Pablo_Ramos
NXP Employee
NXP Employee

Hi,

You can refer to the following community post, in there you will find an explanation of how to switch between heap implementations.

Solved: Re: FreeRTOS, LWIP, MEBDTLS - NXP Community

 

0 件の賞賛
返信