Lwip and heap4.c in freertos

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Lwip and heap4.c in freertos

跳至解决方案
499 次查看
andréluis
Contributor II

Hi, I'm using a MIMXRT1060-EVK. I have an application running lwIP with FreeRTOS, using heap_3. But I need to change my application to run in FreeRTOS with heap_4. When I made the changes, I can build and debug, but I don't even receive a ping. Is there some configuration I need to do to make it work? Thanks for the help.

0 项奖励
回复
1 解答
430 次查看
Pablo_Ramos
NXP Employee
NXP Employee

Hi,

You can refer to the following community post, in there you will find an explanation of how to switch between heap implementations.

Solved: Re: FreeRTOS, LWIP, MEBDTLS - NXP Community

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
431 次查看
Pablo_Ramos
NXP Employee
NXP Employee

Hi,

You can refer to the following community post, in there you will find an explanation of how to switch between heap implementations.

Solved: Re: FreeRTOS, LWIP, MEBDTLS - NXP Community

 

0 项奖励
回复