Lpspi slave transmission error with Yocto and i.mx8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lpspi slave transmission error with Yocto and i.mx8

1,660 Views
s233199
Contributor II

Hello, I have a problem with my lpspi slave driver. I am using the i.mx8qmlpddr4arm2 board with Yocto Morty. I added lpspi slave support from newer kernel, in particular I am using this version of lpspi driver: https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/spi/spi-fsl-lpspi.c?h=imx_4.14.78_...

To make the system work correcty in my board I have modified the interrupt service routine of the driver:

static irqreturn_t fsl_lpspi_isr(int irq, void *dev_id)
{
    u32 temp_SR, temp_IER;
    struct fsl_lpspi_data *fsl_lpspi = dev_id;

    temp_IER = readl(fsl_lpspi->base + IMX7ULP_IER);
    fsl_lpspi_intctrl(fsl_lpspi, 0);
    temp_SR = readl(fsl_lpspi->base + IMX7ULP_SR);

    fsl_lpspi_read_rx_fifo(fsl_lpspi);

    if ((temp_SR & SR_TDF) && (temp_IER & IER_TDIE)) {
        fsl_lpspi_write_tx_fifo(fsl_lpspi);
        return IRQ_HANDLED;
    }

    if (temp_SR & SR_RDF && (temp_IER & IER_RDIE)) {
        complete(&fsl_lpspi->xfer_done);
        return IRQ_HANDLED;
    }

    return IRQ_NONE;
}

and the function write_tx_fifo:

static void fsl_lpspi_write_tx_fifo(struct fsl_lpspi_data *fsl_lpspi)
{
    u8 txfifo_cnt;
    u32 temp;

    txfifo_cnt = readl(fsl_lpspi->base + IMX7ULP_FSR) & 0xff;

    while (txfifo_cnt < fsl_lpspi->txfifosize) {
        if (!fsl_lpspi->remain)
            break;
        fsl_lpspi->tx(fsl_lpspi);
        txfifo_cnt++;
    }

    if (txfifo_cnt < fsl_lpspi->txfifosize) {
        if (!fsl_lpspi->is_slave) {
            temp = readl(fsl_lpspi->base + IMX7ULP_TCR);
            temp &= ~TCR_CONTC;
            writel(temp, fsl_lpspi->base + IMX7ULP_TCR);
        }
        fsl_lpspi_intctrl(fsl_lpspi, IER_RDIE);
    } else
        fsl_lpspi_intctrl(fsl_lpspi, IER_TDIE);
}

My board in slave mode can comunicate with another board, and the data received is correct, but when I perform two consecutive transfers, the words received in the second one are read one word late, I mean it seems that the transmit fifo is not loaded in time so when a word arrives I am still loading the transmit fifo and the receive interrupt do not fire. It is weird because the data is sent one word each second, which is a lot of time. I have tried with clock speed at 100k hz, 200k hz and 500k hz.

What could be the reason of this behaviour? And how could I adjust it?

Thanks a lot,

Erica

0 Kudos
Reply
5 Replies

1,489 Views
igorpadykov
NXP Employee
NXP Employee

Hi Erica

seems you are using very old L4.9.51-beta2 release which has not full i.MX8QM support.

Recommended to use latest L4,14,98 sumo with latest patches from i.MX Software | NXP 

linux-imx - i.MX Linux kernel 

Linux L4.14.98_2.0.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,489 Views
s233199
Contributor II

Thank you Igor. In the Yocto project's user's guide, in the build configurations there is not my board imx8qmlpddr4arm2. I have tried to use Yocto sumo for this board in the past but after flashing the image the board couldn't boot. I was able to boot only using Yocto morty. Is this problem fixed now?

Regards,

Erica

0 Kudos
Reply

1,489 Views
igorpadykov
NXP Employee
NXP Employee

Hi Erica

seems you are using old i.MX8QM revision which was supported only on

early linux releases. Suggest to use latest silicon revision which is supported

by sumo.

pastedImage_2.jpg

i.MX Software | NXP 

Best regards
igor

0 Kudos
Reply

1,489 Views
s233199
Contributor II

Hi Igor, in all the guides I only read imx8qmmek.Can I use it for the board imx8qmlpddr4amr2?

0 Kudos
Reply

1,489 Views
igorpadykov
NXP Employee
NXP Employee

Hi Erica

 imx8qmlpddr4amr2 is internal validation board not intended for customer use.

So it is not formally supported.

Best regards
igor

0 Kudos
Reply