Low power surveillance camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Low power surveillance camera

552 Views
Kuntalaman
Contributor II

Hello Guys greetings,

i am designing a ultra low power battery operated surveillance camera.

Expectation:

1. 5-12 MP camera support with 720p-1080p resolution 

2. Image capturing and video recording features along with audio recording 

3. Should have various low power modes

4. boot up time 200ms

5. current consumption while recording video should be 200-300mA or 324mW at 1.2V

6. Basically it should consume less current.

these are my requirements, can anyone suggest Me better soc for my this project, which satisfies or meet my expectations 

 

0 Kudos
Reply
6 Replies

517 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes you can try the iMX93, that with the OV5640 at 5MP on 720p we get 200 mA

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

Regards

0 Kudos
Reply

508 Views
Kuntalaman
Contributor II

and please provide solution for all asked question 

0 Kudos
Reply

510 Views
Kuntalaman
Contributor II

But OV5640 is not a low light sensor, as it doesn't give clear picture in night operations, what about 7ULP or 8ULP

0 Kudos
Reply

511 Views
Kuntalaman
Contributor II
But OV5640 is not better sensor for low light operations
0 Kudos
Reply

505 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, as well the OV5640 is supported by MX7ULP, if you want to see how much it consumes with your camera you have to build your driver.

Regards

0 Kudos
Reply

503 Views
Kuntalaman
Contributor II
I can built that, but suggest me best low power consumption based soc, along with boot up time 200ms
0 Kudos
Reply