Hi,
I dont want use echo mem > /sys/power/state because i cant wakeup system after with a GPIO and how reduce the consumption via software with for example (reduce the frequency of the CPU and shutdown the various peripherals)?
how modified mx53_loco.c for to obtaine reduced consumption and which register i must modified? there is an example?
For example I'm trying to turn off all clock with CCM_CCGR register, but i dont know how to do..
I've inserted this code in my mx53_loco.c:
_clk_disable(&pll1_sw_clk) but i have same error...
thanks..
do you have QQ?
Recommend that you have posted the questions into imxcommunity. So you can get more supports from the whole world.
Regarding the brightness control code, you can use:
fopen – Open backlight sys file
fread – get backlight
fprintf – write new backlight file
fclose
You mean you hope to reduce MX53 power in idle/normal case?
If you want to switch CPU, you can use enable DVFS to do CPU frequency switch with voltage change:
To Enable the DVFS core use this command:
echo 1 > /sys/devices/platform/mxc_dvfs_core.0/enable
To Disable The DVFS core use this command:
echo 0 > /sys/devices/platform/mxc_dvfs_core.0/enable
As you mentioned, you can close the clocks which are not used in our cases.
You can also disable the modules which are not used or put them into low memory modes according to spec.
ok thanks,
but how close the clocks which are not used?
you can write a little example?
You can call function “clk_disable”.
Please note you should ensure clk_enable and clk_disable keep pair.
Meanwhile, you can also use memtool to dump CCM register bits for CG bit. And ensure the required clocks are closed really for debug purpose.
ok and how disable also pwm?
in stanby state i note that pwm of my backlight is max value (0) i want that it's 255.
I've view in pwm_bl.c this function:
#ifdef CONFIG_PM
static int pwm_backlight_suspend(struct platform_device *pdev,pm_message_t state);
Now how use it in pm.c?
pwm_backlight_suspend(struct platform_device *pdev,pm_message_t state);
What i must put at "struct platform_device *pdev" and pm_message_t state?
i want disable pwm.0 and in mx53_loco.c I have this:
static struct platform_pwm_backlight_data mxc_pwm_backlight_data= {
.pwm_id = 1,
.max_brightness = 255,
.dft_brightness = 128,
.pwm_period_ns = 50000,
};
For pwm backlight, you can control from user space through sys.
Suspend:
echo 0 > /sys/class/backlight/pwm-backlight.0/brightness
Then restore to original value after resume.
To disable PWM0, please remove PWM Pin configuration firstly. Then remove relative driver register into the board files.
yes i know this:
but at start:
cat /sys/class/backlight/pwm-backlight.0/brightness
128
after
echo mem > /sys/power/state
i view that brigthness is max (seems that standby do echo 255 > /sys/class/backlight/pwm-backlight.0/brightness).
One common way is:
1. Get current backlight in user space.
2. Then set as new value for suspend.
3. Suspend.
4. Resume
5. Restore to early stored value.
You can add the logs in pwm_bl.c to debug the issue you observed. And see whether brightness is changed or not.
cat /sys/class/backlight/pwm-backlight.0/brightness
128
Then set as new value for suspend. <--how?
echo mem > /sys/power/state <-- i view backlight at max
resume:
cat /sys/class/backlight/pwm-backlight.0/brightness
128
i think that in pm.c i must call pwm_backlight_suspend(struct platform_device *pdev,pm_message_t state); but how?
you can write an example for me thanks?
nothing?