What is the lowest cost i.mx6 development board that supports a camera interface with four lanes of MIPI-CSI2?
Also, I need it to have Yocto support.
Thank you,
Bob
Having looked at this a little more, I'm also open to using something other than i.MX6. i.MX8 may be the better choice. The important thing here is a robust CSI-2 connector, an existing camera to test it with, and good Yocto support.
for i.MX8 one can look on
i.MX 8 Series Applications Processors | Arm® Cortex®-A72/A53/A35/M4 cores | NXP
click on processor, then on "Development Boards" on left side of page
Best regards
igor
Hi Robert
for low cost boards one can look for example on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you Igor. This might work.
I was looking at the EDM-iMX6 schematic, and on page 6 it shows a MIPI Camera Connector: FP124-334M4.
I searched on this connector, but it came up empty. If we buy your board(s), we need to interface to the connector. Please let me know who makes it and what it will mate with (e.g., cable). Being able to mate with the connector to a board my company is building is a critical issue.
http://download.wandboard.org/wandboard-imx6/documentation/wbquad-revb1-userguide.pdf
Thanks,
Bob
Hi Robert
these boards are not supported by NXP, this may be posted on Wandboard Wiki
NXP supports only own i.MX6 reference boards, like Sabre SD, Sabre AI :
i.MX Evaluation and Development Boards | NXP
Best regards
igor