Lost usb data caused by print debug message on imx51 evk on windows embedded compact 7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Lost usb data caused by print debug message on imx51 evk on windows embedded compact 7

957 次查看
謝端桂
Contributor I

Dear all:

I create a thread to receive usb data from touch screen. My data is separately in two packet in sometimes.

I will lost usb data, When print more debug messages. It seem likely timing issue. Does anybody encounter this problem?

I care about this problem. If I add some code in the thread, it will lead to the same situation. Does anybody have solution?

best regards,

Victor

标签 (2)
0 项奖励
回复
1 回复

859 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

The physical memory for these transfer buffers is allocated as a pool at driver initialization. Unless physical addresses are specified in API accesses at the class-driver interface, the driver copies data between the user/class-provided data buffers and the DMA buffer from the driver physical memory pool, if you think that the issue is due to Wince or Mx51 Hardware side you should try to isolate the issue, check the USB transfer with a USBsniffer or with the CTK test  refer to :

Windows Embedded Compact 7 > Compact Test Kit(CTK)

hope this helps

0 项奖励
回复