Looking for assistance in connecting a motion sensor and camera module to the IMX53 Quickstart board.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Looking for assistance in connecting a motion sensor and camera module to the IMX53 Quickstart board.

829 次查看
den_den
Contributor I

 

I am looking for assistance in connecting a motion-sensor and camera to the IMX hardware. In particular, the IMX53 Quickstart board.

 

The motion sensor would act as event generator for the IMX hardware. As soon the motion is detected, IMX receives the interrupt and initiates the camera to capture the motion.

 

The goal is to capture video/images in less that 500ms.

 

Apart from the hardware design, I would need the source code (Firmware / OS / application software) that is required for these device feature to work as per given sla.

 

标签 (1)
标记 (3)
0 项奖励
回复
0 回复数