Logcat crashes with error: unexpected EOF in Android 9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Logcat crashes with error: unexpected EOF in Android 9

ソリューションへジャンプ
4,711件の閲覧回数
vinothkumars
Senior Contributor IV

Dear NXP,

 

I am working on i.MX 6Quad SABRE-SD with Android 9. Logcat crashing after increment the buffer size also. I configured buffer size to 200Mb.

logcat -G 200Mb (before 64 Kb)

But, even though I got the EOF error. 

Is there any other configuration do we need to for increase buffer size automatically ?

Thanks & Regards,

VinothS.

Regards,
Vinothkumar Sekar
ラベル(2)
タグ(4)
0 件の賞賛
返信
1 解決策
4,377件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

This is caused by the lack of RAM memory in the sabreSD board. Unfortunately, a buffer of 200MB is a lot for the i.MX 6Quad SABRE-SD since the board only has 1 GB of RAM. I apologize for the inconvenience this could give you.

Best regards,

Diego.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,378件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

This is caused by the lack of RAM memory in the sabreSD board. Unfortunately, a buffer of 200MB is a lot for the i.MX 6Quad SABRE-SD since the board only has 1 GB of RAM. I apologize for the inconvenience this could give you.

Best regards,

Diego.

0 件の賞賛
返信
4,377件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you Diego,

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 件の賞賛
返信