Lock up when configuring irq for IRQF_TRIGGER_HIGH on iMX6 saberlite board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Lock up when configuring irq for IRQF_TRIGGER_HIGH on iMX6 saberlite board

1,147 次查看
anilghadiya
Contributor II

Hi,

We are trying to configure one of the GPIO(205) pin to generate interrupt when level is HIGH on the pin.

So we Have passed IRQF_TRIGGER_HIGH flag while registering the isr using request_irq(). But After this, Module is not getting inserted.

Is there any configuration which is required to generate the level based interrupt.

Thanks in advance,

Anil Patel

标签 (2)
0 项奖励
回复
0 回复数