Location of IOMUX Tool for i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Location of IOMUX Tool for i.MX6UL

Jump to solution
4,355 Views
ko-hey
Senior Contributor II

Hi all

Where is a IOMUX Tool for i.MX6UL ?

I downloaded IOMUX Tool from following page but it wasn't included.

IOMUX Tool Introduction

Ko-hey

Tags (2)
0 Kudos
Reply
1 Solution
1,984 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the Processor Expert instead.

For the 6UL the IOMUX tool functionality has been rolled into the Processor Expert tool for i.MX6.
There is no separate IOMUX tool.


An update has to be applied for the i. MX6UL.

http://cache.freescale.com/lgfiles/devsuites/PEx/PEx_i.MX_6UL_Eclipse_Update_unzip_me.zip


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
7 Replies
1,984 Views
BiyongSUN
NXP Employee
NXP Employee

Since SoloX the pin mux is support by Processor Expert for i.MX.

Processor Expert for i.MX|Freescale

Untitled.png

1,984 Views
Danube
Contributor IV

Hi Sir,

Do you have i.MX6UL pin mux excel file ?

Process Expert can't copy all pin to excel file.

0 Kudos
Reply
1,984 Views
ko-hey
Senior Contributor II

Hi Yuri and Biyong

Thanks, I'll try it.

Ko-hey

0 Kudos
Reply
1,985 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the Processor Expert instead.

For the 6UL the IOMUX tool functionality has been rolled into the Processor Expert tool for i.MX6.
There is no separate IOMUX tool.


An update has to be applied for the i. MX6UL.

http://cache.freescale.com/lgfiles/devsuites/PEx/PEx_i.MX_6UL_Eclipse_Update_unzip_me.zip


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,984 Views
wowa
Contributor I

Hi All,

Hi Yuri,

i am not a software developer. I have no idea about eclipse.... So for me it is very difficult to use "Expert" instead of IOMUX Tool.

Does exist a "HowTo" for beginners or a easier way to check the pin configuration ?

I only want to see if my configuration with my wished functions is working or not.... In IOMUX you could see e.g.

in a diagram if you get a conflict or not....

Thanks for help beforehand.

0 Kudos
Reply
1,984 Views
Yuri
NXP Employee
NXP Employee

Hello,

Basically You may manually check pin mux configuration, using section 4.1.1 (Muxing Options)

of the i.MX6UL RM.

Regards,

Yuri.

0 Kudos
Reply
1,984 Views
wowa
Contributor I

Hi,

but It is very complex with this method. I have solved the issue with PE right now.

If you are accustomed to work with IOmux tool the PE is a new world for HW-Developers.

Thanks.

Regards.

Wolfgang

0 Kudos
Reply