Hi all
Where is a IOMUX Tool for i.MX6UL ?
I downloaded IOMUX Tool from following page but it wasn't included.
Ko-hey
Solved! Go to Solution.
Hello,
Please use the Processor Expert instead.
For the 6UL the IOMUX tool functionality has been rolled into the Processor Expert tool for i.MX6.
There is no separate IOMUX tool.
An update has to be applied for the i. MX6UL.
http://cache.freescale.com/lgfiles/devsuites/PEx/PEx_i.MX_6UL_Eclipse_Update_unzip_me.zip
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Sir,
Do you have i.MX6UL pin mux excel file ?
Process Expert can't copy all pin to excel file.
Hi Yuri and Biyong
Thanks, I'll try it.
Ko-hey
Hello,
Please use the Processor Expert instead.
For the 6UL the IOMUX tool functionality has been rolled into the Processor Expert tool for i.MX6.
There is no separate IOMUX tool.
An update has to be applied for the i. MX6UL.
http://cache.freescale.com/lgfiles/devsuites/PEx/PEx_i.MX_6UL_Eclipse_Update_unzip_me.zip
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi All,
Hi Yuri,
i am not a software developer. I have no idea about eclipse.... So for me it is very difficult to use "Expert" instead of IOMUX Tool.
Does exist a "HowTo" for beginners or a easier way to check the pin configuration ?
I only want to see if my configuration with my wished functions is working or not.... In IOMUX you could see e.g.
in a diagram if you get a conflict or not....
Thanks for help beforehand.
Hello,
Basically You may manually check pin mux configuration, using section 4.1.1 (Muxing Options)
of the i.MX6UL RM.
Regards,
Yuri.
Hi,
but It is very complex with this method. I have solved the issue with PE right now.
If you are accustomed to work with IOmux tool the PE is a new world for HW-Developers.
Thanks.
Regards.
Wolfgang