Load software to the two ARM Cortex inside the iMX8 SoC in Google's Coral SoM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Load software to the two ARM Cortex inside the iMX8 SoC in Google's Coral SoM

230 Views
DevElec
Contributor II

Hello!

I want to know how can I load software or programme the two microprocessors inside the SoC in the Google's Coral System-on-Module: NXP i.MX 8M SoC (quad Cortex-A53, Cortex-M4F). I don't how to load code in this components or even if this is possible or they are managed by the SoM for some processes without the possibility of programming them apart.

My idea is to use this microprocessors as controllers of a process that will launch the TPU eventually, but I have no idea about how to load the software in these ARMs inside the SoC (if it is possible).

Thank you.

0 Replies