Linux zImage riotboard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux zImage riotboard

2,241件の閲覧回数
erikfriesen
Contributor II

As near as I know, I have followed these steps

RIoTboard: Linux on the RIoTBoard Part 2: Kernel | element14

The first time on a digital ocean server everything worked as expected.  I have zipped the linux build and transferred it to a local machine, and now the device won't boot anyway I can figure out.

After putting the new zImage in /boot/ I get this

Hit any key to stop autoboot:  0

MMC: no card present

MMC: no card present

switch to partitions #0, OK

mmc2(part 0) is current device

Scanning mmc 2:1...

Found U-Boot script /boot.scr

293 bytes read in 137 ms (2 KiB/s)

## Executing script at 13100000

switch to partitions #0, OK

mmc2(part 0) is current device

5690392 bytes read in 370 ms (14.7 MiB/s)

31992 bytes read in 61 ms (511.7 KiB/s)

Kernel image @ 0x10800000 [ 0x000000 - 0x56d418 ]

## Flattened Device Tree blob at 16800000

   Booting using the fdt blob at 0x16800000

   Loading Device Tree to 1fff5000, end 1ffffcf7 ... OK

Starting kernel ...

Changing the boot.scr to boot a uImage, I get this

U-Boot 2015.10-rc3-00214-g8a5f612 (Sep 23 2015 - 07:16:49 -0400)

CPU:   Freescale i.MX6SOLO rev1.1 996 MHz (running at 792 MHz)

CPU:   Commercial temperature grade (0C to 95C) at 40C

Reset cause: WDOG

Board: RIoTboard

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

No panel detected: default to HDMI

Display: HDMI (1024x768)

In:    serial

Out:   serial

Err:   serial

Net:   FEC [PRIME]

Error: FEC address not set.

Hit any key to stop autoboot:  0

MMC: no card present

MMC: no card present

switch to partitions #0, OK

mmc2(part 0) is current device

Scanning mmc 2:1...

Found U-Boot script /boot.scr

313 bytes read in 138 ms (2 KiB/s)

## Executing script at 13100000

Unknown command 'bootscript' - try 'help'

switch to partitions #0, OK

mmc2(part 0) is current device

5690456 bytes read in 356 ms (15.2 MiB/s)

31992 bytes read in 61 ms (511.7 KiB/s)

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    5690392 Bytes = 5.4 MiB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 16800000

   Booting using the fdt blob at 0x16800000

   Loading Kernel Image ... OK

   Loading Device Tree to 1fff5000, end 1ffffcf7 ... OK

Starting kernel ...

So is there some factor I am missing here?

If its is a factor, emdebian doesn't host the toolchain anymore, could the gcc be a factor here?  I did an apt-get install gcc-arm-linux-gnueabihf

ラベル(1)
2 返答(返信)

1,894件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Erick,

It is not clear the procedure you follow up to Zip the zImage, Generally zImage is not too big to be zipped, I suggest not compress this file and copy/paste directly to the device. If in any case you suspect of the gcc toolchain, please download a try with linaro toolchain such as:

https://releases.linaro.org/14.09/components/toolchain/binaries/gcc-linaro-arm-linux-gnueabihf-4.9-2...

hope this helps

0 件の賞賛
返信

1,894件の閲覧回数
erikfriesen
Contributor II

I zipped it using bzImage.

In the end it was a combination of compiler and some obscure option I must have had wrong.  Updated to linaro 4.9, called make imx_v6_v7_defconfig to reset the options, and it worked.