Linux patch to support 8GB NAND flash on iMX53 (MT29F64G08AJABA(8GB), 2CE) -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux patch to support 8GB NAND flash on iMX53 (MT29F64G08AJABA(8GB), 2CE) -blog archive

2,472 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

The default Linux BSP has issues to support the 8GB NAND, the attached is the patch to fix it, all modified codes are marked with flag "qiang_debug".

 

 

 

Both uboot. kernel and mtd-utilis need be updated.

 

In Uboot, "nand erase" can erase the whole NAND.

 

Nand partition in mx53_evk.c is:
static struct mtd_partition nand_flash_partitions[] = {
/* MX53 ROM require the boot FCB/DBBT support which need
* more space to store such info on NAND boot partition.
* 16M should cover all kind of NAND boot support on MX53.
*/
   {
    .name = "bootloader",
    .offset = 0,
    .size = 16 * 1024 * 1024},
   {
    .name = "nand.kernel",
    .offset = MTDPART_OFS_APPEND,
    .size = 5 * 1024 * 1024},
   {
    .name = "nand.rootfs",
    .offset = MTDPART_OFS_APPEND,
    .size = 256 * 1024 * 1024},
   {
    .name = "nand.userfs1",
    .offset = MTDPART_OFS_APPEND,
    .size = 256 * 1024 * 1024},
   {
    .name = "nand.userfs2",
    .offset = MTDPART_OFS_APPEND,
    .size = MTDPART_SIZ_FULL},
};

 

In linux rootfs, I used the followed commands for NAND:
flash_eraseall /dev/mtd2
ubiattach /dev/ubi_ctrl -m 2 -d 2
ubimkvol /dev/ubi2 -n 0 -N rootfs -m
mkdir -p /mnt/ubi2; mount -t ubifs ubi2_0 /mnt/ubi2

 

flash_eraseall /dev/mtd3
ubiattach /dev/ubi_ctrl -m 3 -d 3
ubimkvol /dev/ubi3 -n 0 -N userfs1 -m
mkdir -p /mnt/ubi3; mount -t ubifs ubi3_0 /mnt/ubi3

 

flash_eraseall /dev/mtd4
ubiattach /dev/ubi_ctrl -m 4 -d 4
ubimkvol /dev/ubi4 -n 0 -N userfs2 -m
mkdir -p /mnt/ubi4; mount -t ubifs ubi4_0 /mnt/ubi4

Original Attachment has been moved to: R10.3.2-Code-update-for-large-NAND_0413.zip

Labels (3)
Tags (1)
0 Kudos
Reply
2 Replies

840 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Maybe you need double check the timing parameters. They can be found in the NAND datasheet.
.data_setup_in_ns = 10,
.data_hold_in_ns = 5,
.address_setup_in_ns = 10,

0 Kudos
Reply

840 Views
HuiShao
Contributor I

Hi Qiang

 

I am working on a customized board based on iMX53 QSB and enabling

MT29F2G08ABBEAH4 NAND via PATA I/F in u-boot. Wondering if you could help.

Here are chip info:

Single-level cell (SLC) technology

• Organization

– Page size x8: 2112 bytes (2048 + 64 bytes)

– Page size x16: 1056 words (1024 + 32 words)

– Block size: 64 pages (128K + 4K bytes)

– Plane size: 2 planes x 1024 blocks per plane

– Device size: 2Gb: 2048 blocks

 

And nand_device_info_table_type_7[] in drivers/mtd/nand/nand_device_info.c       

{

        .end_of_table             = false,

        .manufacturer_code        = 0x2c,

        .device_code              = 0xaa,

        .cell_technology          = NAND_DEVICE_CELL_TECH_SLC,

        .chip_size_in_bytes       = 256LL*SZ_1M,

        .block_size_in_pages      = 64,

        .page_total_size_in_bytes = 2*SZ_1K + 64,

        .ecc_strength_in_bits     = 4,

        .ecc_size_in_bytes        = 512,

        .data_setup_in_ns         = 10,

        .data_hold_in_ns          = 5,

        .address_setup_in_ns      = 10,

        .gpmi_sample_delay_in_ns  = 6,

        .tREA_in_ns               = -1,

        .tRLOH_in_ns              = -1,

        .tRHOH_in_ns              = -1,

        "MT29F2G08ABBEAH4",

        },

 

What i got is NAND probe is OK but read/write/erase are all failed:

MX53-CSSU U-Boot > nand device

Device 0: NAND 256MiB 1,8V 8-bit, sector size 128 KiB

 

MX53-CSSU U-Boot > nand erase 0x20000 0x20000

NAND erase: device 0 offset 0x20000, size 0x20000

NAND 256MiB 1,8V 8-bit: MTD Erase failure: -5

OK

 

MX53-CSSU U-Boot > nand write 0xf8006000 0x0 0x20000

NAND write: device 0 offset 0x0, size 0x20000

nand_do_write_ops: Device is write protected NAND write to offset 0 failed -5

0 bytes written: ERROR

 

MX53-CSSU U-Boot > nand read 0xf8006000 0x0 0x20000

NAND read: device 0 offset 0x0, size 0x20000

UnCorrectable RS-ECC Error

UnCorrectable RS-ECC Error

UnCorrectable RS-ECC Error

UnCorrectable RS-ECC Error

...

UnCorrectable RS-ECC Error

131072 bytes read: OK

 

Do you have any hints? Thanks in advance,

 

Hui

0 Kudos
Reply