Linux driver of ”Qualcomm AR8035”

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux driver of ”Qualcomm AR8035”

6,977 Views
t_kaz
Contributor I

I want a Linux device driver[source code] for "Qualcomm AR8035" .

According to the following URL, I think driver is being provided by Freescale.

Where can I get that?


http://linux-kernel.2935.n7.nabble.com/PATCH-net-phy-Add-Atheros-AR8035-PHY-support-td637283.html


[Target H/W and SW]

Device : i.mx6 solo

PHY: Qualcomm AR8035

OS: linux 3.0.35

Labels (1)
0 Kudos
Reply
4 Replies

3,760 Views
jamesbone
NXP TechSupport
NXP TechSupport

Our BSP has support for the AR6003, since we recommend to use in our SDP board the SD-SCAN board from Silex,

Here is the link:

http://www.silexamerica.com/campaign/freescale-partner-page/

Have a nice day sir!

0 Kudos
Reply

3,760 Views
t_kaz
Contributor I

Thank you,


Where can I get "Driver for Atheros PHYs"?

Please tell me if you know it.

According to the following URL, I think driver is being provided by Freescale.


http://linux-kernel.2935.n7.nabble.com/PATCH-net-phy-Add-Atheros-AR8035-PHY-support-td637283.html

0 Kudos
Reply

3,760 Views
t_kaz
Contributor I

Thank you for your reply,

Our customer already made the board using AR8035.

Is the driver of AR8035 provided from Freescale?

0 Kudos
Reply

3,760 Views
emestee
Contributor I

Hi,

The AR8035 PHY is used by SolidRun's Cubox-i product, the patched kernel tree is at http://github.com/SolidRun/linux-imx6.git

0 Kudos
Reply