Linux 3.14 hang at reboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux 3.14 hang at reboot

1,358 Views
emilmyhrman
Contributor IV

Using 3.14 kernel and Lollipop 5.1 we sometimes get a hang at "reboot bootloader" command.

I was able to capture this with JTAG.

#0  v7wbi_flush_kern_tlb_range () at arch/arm/mm/tlb-v7.S:84

#1  0xc00160a0 in flush_tlb_kernel_range (start=<optimized out>, end=<optimized out>) at arch/arm/kernel/smp_tlb.c:199

#2  0xc0124fcc in __purge_vmap_area_lazy (start=<optimized out>, end=0xce06dd8c, sync=<optimized out>, force_flush=<optimized out>) at mm/vmalloc.c:636

#3  0xc0125238 in try_purge_vmap_area_lazy () at mm/vmalloc.c:655

#4  free_vmap_area_noflush (va=<optimized out>) at mm/vmalloc.c:678

#5  0xc01253c0 in free_unmap_vmap_area_noflush (va=<optimized out>) at mm/vmalloc.c:688

#6  free_unmap_vmap_area (va=0xc44b3940) at mm/vmalloc.c:697

#7  0xc0126c28 in remove_vm_area (addr=<optimized out>) at mm/vmalloc.c:1419

#8  0xc0126c78 in __vunmap (addr=0xbf00a000, deallocate_pages=-364908544) at mm/vmalloc.c:1438

#9  0xc0126ea8 in vunmap (addr=0xbf00a000) at mm/vmalloc.c:1513

#10 0xc001d760 in __iounmap (io_addr=<optimized out>) at arch/arm/mm/ioremap.c:429

#11 0xc001d6c4 in __arm_iounmap (io_addr=<optimized out>) at arch/arm/mm/ioremap.c:436

#12 0xc00216bc in do_switch_fastboot () at arch/arm/mach-imx/system.c:111

#13 0xc0021830 in arch_reset_special_mode (mode=<optimized out>, cmd=<optimized out>) at arch/arm/mach-imx/system.c:121

#14 mxc_restart (mode=<optimized out>, cmd=0xce06de88 "bootloader") at arch/arm/mach-imx/system.c:137

#15 0xc000fbf0 in machine_restart (cmd=0xce06de88 "bootloader") at arch/arm/kernel/process.c:292

#16 0xc005f34c in kernel_restart (cmd=0xce06de88 "bootloader") at kernel/reboot.c:143

#17 0xc005f68c in SYSC_reboot (arg=<optimized out>, cmd=<optimized out>, magic2=<optimized out>, magic1=<optimized out>) at kernel/reboot.c:265

#18 SyS_reboot (magic1=-18751827, magic2=<optimized out>, cmd=<optimized out>, arg=-1095332841) at kernel/reboot.c:199

Any idea what is going on?

Labels (4)
0 Kudos
3 Replies

737 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Emil,

We are internally reviewing your case.

I will post an update as soon as having news.

Best regards!

/Carlos

0 Kudos

737 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Emil,

Can you provide more information? Where do you reboot? What board?

It is best to provide all the log.

Best regards!

/Carlos

0 Kudos

737 Views
emilmyhrman
Contributor IV

Sorry for the late reply.

The board is a custom imx6DL, running Android 5.1.1. This occured when rebooting, e.g. from command line "reboot bootloader".

I never found out why, but worked around this by removing the "iounmap(addr);" in do_switch_recovery (arch/arm/mach-imx/system.c).

0 Kudos